Skip to main content
OPetr.2
Associate II
Aug 22, 2023 2:17 PM UTC
Question

mmc-spi error on STM32MP135-DK

We are using STM32MP135-DK and we connect to SPI5 an SD Card Adapter.

We modified the device tree as follows to use the mmc-spi-slot driver:

 

&spi5{
    pinctrl-names = "default", "sleep";
    pinctrl-0 = <&spi5_pins_mx>;
    pinctrl-1 = <&spi5_sleep_pins_mx>;
    status = "okay";

    /* USER CODE BEGIN spi5 */
     spisdcard@0 {
        compatible = "mmc-spi-slot";
        reg = <0>;
        gpios = <&gpiog 1 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
        voltage-ranges = <3300 3300>;
        spi-max-frequency = <2400000>;
        status = "okay";
        disable-wp;
      };
    /* USER CODE END spi5 */
};

 
but we get this error on startup:
 
OPetr2_0-1692712733832.png

Could you help me to find what is wrong? We checked all the wiring and it is correct.

 
 

 

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
Sep 4, 2023 12:57 PM UTC

Hi @OPetr.2 ,

 

Can you please share the node spi5_pins_mx ? 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
OPetr.2
OPetr.2Author
Associate II
Sep 5, 2023 1:35 PM UTC

Hi @Olivier GALLIEN,  the spi5_pins_mx node in device tree is as follow:

   spi5_pins_mx: spi5_mx-0 {
        pins {
            pinmux = <STM32_PINMUX('A', 8, AF5)>, /* SPI5_MISO */
<STM32_PINMUX('H', 3, AF5)>, /* SPI5_MOSI */
<STM32_PINMUX('H', 7, AF6)>, /* SPI5_SCK */
<STM32_PINMUX('H', 11, AF1)>; /* SPI5_NSS */
            bias-disable;
            drive-push-pull;
            slew-rate = <2>;
        };
    };