Skip to main content
Associate
Jan 10, 2025 3:45 PM UTC
Solved

make[1]: *** No rule to make target 'Image.gz'. Stop.

I've followed the READMEs for the installation of the dev package, source, and kernel and generated a build folder for the kernel as suggested at

~/st/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sdk/Developer-Package/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sources/aarch64-ostl-linux/linux-stm32mp-6.6.48-stm32mp-r1-r0/build

In the build folder I see folders include, scripts, a link to source as well as files Makefile, .config .config.old, and .gitignore. When I run

make ${IMAGE_KERNEL} vmlinux dtbs LOADADDR=0xC2000040 O="${OUTPUT_BUILD_DIR}"

I get

make[1]: *** No rule to make target 'Image.gz'. Stop.
make: *** [/home/lelory/st/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sdk/Developer-Package/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sources/aarch64-ostl-linux/linux-stm32mp-6.6.48-stm32mp-r1-r0/linux-6.6.48/Makefile:234: __sub-make] Error 2

What am I doing wrong?

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
Jan 10, 2025 5:11 PM UTC

Hi,

did the SDK correctly installed and the environment sourced ?

https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-EV1/Develop_on_Arm%C2%AE_Cortex%C2%AE-A35/Install_the_SDK#Start_the_SDK_up

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

2 replies

PatrickF
PatrickFBest answer
ST Employee
Jan 10, 2025 5:11 PM UTC
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Galahad25Author
Associate
Jan 10, 2025 9:29 PM UTC

Ah, didn't realize I had to source when changing folders as well. Now another issue:

/home/lelory/st/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sdk/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/lib/aarch64-ostl-linux/gcc/aarch64-ostl-linux/13.3.0/plugin/include/builtins.h:23:10: fatal error: mpc.h: No such file or directory
23 | #include <mpc.h>

It doesn't show the file in the gcc and I don't see it there either.