Skip to main content
meiss.M
Associate III
Jul 9, 2020 8:18 AM UTC
Solved

M4 ELF build done in CUBEIDE is not uploaded to target on dunfell platform

The program can not be uploaded under the dunfell distribution via CUBEIDE 1.3.1 to the target system. Using the thud distribution, target uploads works.

Are there any hidden upload scripts in the CUBEIDE - how to debug the debug upload?

Which yocto packages are necessary to cooperate with the CUBEIDE?

This topic has been closed for replies.
OlivierK
OlivierKBest answer
ST Technical Moderator
Jul 17, 2020 2:32 PM UTC

Hi,

​The fix is now published.

https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note_-_v2.0.0

https://wiki.st.com/stm32mpu/wiki/STM32MP15_OpenSTLinux_release_note_-_v2.0.0

some cipher methods have been disabled by the community for security reasons.

As a consequence some ssh requests from STM32CubeIDE may not be functional due to the dropbear package configuration.

In this case, you can either:

Best Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

23 replies

meiss.M
meiss.MAuthor
Associate III
Jul 20, 2020 10:34 AM UTC

Hi Oliver,

thanks for adding this to upstream.

Did you check firmware upload from STMcubeIDE if the the target is missing the directory /lib/firmware.

On my system, firmware upload works, however, a symlink is created:

lrwxrwxrwx   1 root    root           92 Feb 7 17:11 /lib/firmware -> /usr/local/projects/MYPROJECT/lib/firmware/MYPROJEKT_CM4.elf

and IDECube fails with the message: Failed to insert hardware breakpoints: You have requested too many hardware breakpoints/watchpoints.

Can you reproduce this.

OlivierK
ST Technical Moderator
Jul 20, 2020 5:01 PM UTC

​Hi  meiss.M (Community Member)

Indeed, I have the same symlink to the .elf.  But I don't get the message regarding the H/w breakpoint. Could you please share your console log?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
meiss.M
meiss.MAuthor
Associate III
Jul 21, 2020 8:59 AM UTC

I can share in a couple of days, since the power controller on our dk2 broke yesterday.