Skip to main content
Associate II
Feb 6, 2024 11:04 AM UTC
Solved

LWIP+RTOS Problem pinging board

Hey, 

I am using STM32F407 and I am trying to configure the ethernet peripheral (and LWIP) with the cubemx with no success. I cant ping my board.

Please anyone can help me with this?

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 6, 2024 11:45 AM UTC

Hello,

Not easy to answer that question based on your description. It could be related to the HW or software (what is the HW you're using: PHY, Clock etc ..)

What I suggest you is to refer to one of the examples provided in STM32CubeF4 under the path Projects\STM324xG_EVAL\Applications\LwIP\LwIP_HTTP_Server_Socket_RTOS

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

2 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 6, 2024 11:45 AM UTC

Hello,

Not easy to answer that question based on your description. It could be related to the HW or software (what is the HW you're using: PHY, Clock etc ..)

What I suggest you is to refer to one of the examples provided in STM32CubeF4 under the path Projects\STM324xG_EVAL\Applications\LwIP\LwIP_HTTP_Server_Socket_RTOS

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate II
Feb 6, 2024 11:58 AM UTC

I am using STM32F407VGT, With a RJ45 connector and ethernet ic which supports LAN8742. These are the configurations i have set MXCube. And just a self generated code from MXcube but not able to ping my board.Which has MX_LWIP_Init in default task.