Skip to main content
mrnuke
Associate II
Aug 10, 2020 2:53 PM UTC
Question

linux-5.4.31 stuck on boot in start_kernel()/arch_cpu_idle()

I'm trying to build linux-5.4.31 for stm32mp1c-ev1 (tag: v5.4-stm32mp-r1). u-boot loads the kernel successfully, but then nothing happens. I've gone in with GDB, and noticed that the kernel is stuck in start_kernel(), and never leaves it.

What is the fix for this?

#0 cpu_v7_do_idle () at arch/arm/mm/proc-v7.S:78

#1 0xc010a1a4 in arch_cpu_idle () at arch/arm/kernel/process.c:71

#2 0xc0158064 in cpuidle_idle_call () at kernel/sched/idle.c:154

#3 do_idle () at kernel/sched/idle.c:263

#4 0xc01583d8 in cpu_startup_entry (state=CPUHP_ONLINE) at kernel/sched/idle.c:355

#5 0xc0acb5b8 in rest_init () at init/main.c:451

#6 0xc0f00a40 in arch_call_rest_init () at init/main.c:573

#7 0xc0f00f10 in start_kernel () at init/main.c:785

#8 0x00000000 in ?? ()

This topic has been closed for replies.

5 replies

mleo
Visitor II
Aug 12, 2020 7:56 AM UTC

Hello @mrnuke​ ,

I only tried to build the kernel from downloaded file:

https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package#Downloading_the_Linux_kernel

following this instructions (patches, configs, ..)

https://github.com/STMicroelectronics/meta-st-stm32mp/blob/dunfell/recipes-kernel/linux/linux-stm32mp/README.HOW_TO.txt

Could you try the same approach?

In the meantime I'll try rebuild the kernel from github.

Best regards,

Milan

mrnuke
mrnukeAuthor
Associate II
Aug 12, 2020 1:12 PM UTC

Hi @mleo​ .

I tried with the tarball. I did apply the patches and config fragments. I got identical results.

mleo
Visitor II
Aug 13, 2020 1:45 PM UTC

Hi @mrnuke​ ,

What version ofu-boot do you use? (It might not be compatible).

And just to be sure, could you share with us complete log?

Regards,

Milan

mrnuke
mrnukeAuthor
Associate II
Aug 13, 2020 10:21 PM UTC

Hi @mleo​ ,

I tried both the u-boot from the meta-st-stm32mp build, and git.denx.de master (commit 99c6953809 ), with the same results.

I noticed that the problem exhibits when using u-boot SPL, but not with TF-A. I went ahead and bisected the stm branch and found the following commit to introduce the issue:

* 21165f3ebcd4 ARM: dts: stm32: move clocks/resets to SCMI resources for stm32mp15

This makes no sense to me. Is there a reason it would work with one bootloader, but not the other?

fpoussin
Associate III
Aug 13, 2020 10:28 PM UTC

I have the exact same problem with the v5.4-stm32mp-r1 github release

I am using vanilla uboot 2020.04

Booting a vanilla kernel works fine, only this one freezes.

Edit: reverting commit 21165f3ebcd4 fixes the problem