Hi @zengyixiang,
Buildroot distribution based on the OpenSTLiux BSP is supported by STMicroelectronics partner Bootlin.
The version of the Buildroot distribution based on the OpenSTLinux BSP delivered with the STM32MPU-ecosystem-v5.0.0 release (Linux kernel v6.1-stm32mp-r1 (v6.1.28)) is documented in the STM32 MPU wiki: https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ecosystem_release_note_-_v5.0.0 (“Buildroot for Arm® Cortex®-A” chapter). You will find this wiki article links to the Buildroot repository dedicated to supporting the STMicroelectronics STM32MP1 platforms, and to the Bootlin technical support. These links might be helpful for you even if you use the v5.1.0 ecosystem release.
The version of the Buildroot distribution based on the OpenSTLinux BSP delivered with the STM32MPU-ecosystem-v5.1.0 release (Linux kernel v6.1-stm32mp-r2 (v6.1.28)) is being built by Bootlin and will be available soon. Once available, it will be documented in the following wiki article: https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ecosystem_release_note_-_v5.1.0 (“Buildroot for Arm® Cortex®-A” chapter): “under construction” for the moment.
Hope this information helps.
Regards,
JC.
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.