Skip to main content
Associate
Dec 11, 2025 9:47 AM UTC
Question

Latest supported version of Chromium

Hello,


I want to know what is the latest Chromium version supported by OpenST Linux on Scarthgap.
Do we have GPU acceleration on it?

Thank you in advance,

Hiba

 

@PPAGE.13

@Billy OWEN 

@Gregory PLANCHON 

6 replies

Lead
Dec 12, 2025 10:41 AM UTC

@hiba 

The ST Dev Team is working on a solution for that. 

They said they will find a solution in half of 2025.

What ST have tried is to build a minimal chromium web browser by using Qt Web Engine, which use the same web engine as Chromium. They have run that Qt Nano Web browser in kiosk mode, e.g no buttons and input text boxes. It works like a charm.

My advice is to look for Gentoo Use flags to see what you can use with compilation for Firefox. They have a lot of flags you can use to optimize a web browser by using the same web engine as Firefox is using.

I'm working on a Github project for creating an optimal web browser for MP2.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
Yassine_behilil
Graduate II
Apr 27, 2026 12:17 PM UTC

 

I am currently working on bringing up Chromium on a custom board based on STM32MP255C, using OpenSTLinux 6.2 (Scarthgap).

Context

  1. Platform: STM32MP255C (custom board)

  2. Distribution: OpenSTLinux 6.2 (Scarthgap)

  3. Goal: Run a Chromium-based browser with GPU acceleration (Wayland/Weston or equivalent)


Questions

  1. Chromium support status

    • What is the latest Chromium version officially supported on OpenSTLinux 6.2 for STM32MP25?

    • Is there any validated configuration for Chromium on this platform?

  2. Layer availability

    • Does ST provide or maintain a Yocto layer (meta-chromium or equivalent) compatible with OpenSTLinux 6.2?

    • If yes, could you share:

      • the repository

      • the branch

      • or the exact commit used internally

  3. GPU acceleration

    • Is GPU acceleration supported with Chromium on STM32MP25?

    • If yes:

      • which backend is expected (Wayland, X11, EGL, Ozone-Wayland, etc.)?

      • are there specific patches or configurations required?

  4. Recommended approach

    • Is Chromium currently a supported use case, or is the recommended approach still:

      • Qt WebEngine

      • or another browser stack?


Additional information

I noticed discussions indicating that Chromium support is still under development for MP25. I would like to understand the current official position and whether there is any internal or experimental layer already available for OpenSTLinux 6.2.


Thank you in advance for your support.

BR,
Yassine 

Lead
May 10, 2026 4:04 PM UTC

@unknown 

Have you tried to build a web browser for STM32MP257?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
asadullah4571
Associate III
Aug 20, 2026 1:06 PM UTC

Hi ​@DMårt , ​@Yassine_behilil , ​@hiba , 

I m still waiting for the chromium support for the stm32mp2 series form last 2 years, they said they will release in mid of 2025, now the mid of 2026, 

they did not response yet, i do not need to much functionality , just video play and some scrolling messages and GIF content.