Skip to main content
asadullah4571
Associate III
Dec 25, 2024 12:28 PM UTC
Question

It's very Hard to Play videos with chromium-wayland on STM32MP257-EV/DK

I have both Board "stm32mp257F-dk - F-ev"

I try to install chromium on the STM32MP2 , and Successfully installed chromium ,
I try to play video on YouTube it is to lagging , smoothly play on 360p only, without YouTube i treid different method to play video on chromium. but also the output same,

is there any thing to reslove this issues?
My project based of Web display with high resolution video upto 1080p60 fps on HDMI .
please give me the update on this, can my project work on this board.

6 replies

PPAGE.13
ST Employee
Jan 27, 2025 11:56 AM UTC

Hi,

today Chromium does not support natively our hardware video decoder on MP2.

We are in the phase to integrate adaptation so that we can get benefit of our hardware acceleration.

It should probably come out in the second half of 2025.

If you need to play high resolution streams, please use gstreamer.

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Lead
Jun 9, 2025 5:15 PM UTC

@asadullah4571 

@PPAGE.13 

I'm very interested in how the status of this integration. Will ST succeed to make sure Chromium to benefit from hardware acceleration? 

When you talking about "gstreamer", you mean that gstreamer could make it possible to play 1080p videos on Youtube with Chromium at STM32MP2?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer