Skip to main content
Associate II
Nov 6, 2025 8:13 AM UTC
Question

Issue running STM32DDRFW-UTIL

Hi team, 

I am able to successfully use pre-build binary from this https://github.com/STMicroelectronics/STM32DDRFW-UTIL.git repo for DDR4 with stm32mp257f-evk . but the generated artifacts with stm32 header by manually compiling in stm32cubeide I am facing the issue, After flashing I am not able to enter any command in the serial monitor window. 
I followed the build procedure explained in the repo's README.md

Vijay_kumar_0-1762416665196.png

As you can see in attached image only this DDR> prompt line is printed in serial port but not accepting any input from user , when I try to enter some command it reinitialized stdin to the same DDR> prompt line.

Thank you in advance...!!
hoping for a quick reply.

 

This topic has been closed for replies.

3 replies

PatrickF
ST Employee
Nov 6, 2025 10:24 AM UTC

Hi,

maybe just a local echo issue.

Did you have set the DDR_INTERACTIVE ?

Did you try blindly typing 'help' to see if any output ?

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Associate II
Nov 7, 2025 9:27 AM UTC

@PatrickF 
Thanks for the reply..
I have setted DDR_INTERACTIVE as per REAMME.md 

Vijay_kumar_0-1762506767479.png

If I am using serial_putchar() I can able to flush data to my promt line but If I am using printf statements i can't getting any terminal output , Its getting stuck there .


I have created my own _write() function , __io_putchar() and tried using __attribute__(( weak )) this function for multiple definitions to make my function as priority.
I am suspecting printf() is not flushing data and getting stuck there it self. Can you help on
this ?

Regards, 

Vijay

 

PatrickF
ST Employee
Nov 7, 2025 3:55 PM UTC

Hi,

code should compile without any modifications. Please clarify you used the default github code as first intent.

Did you ensure the specific aarch64 prerequisites has been made ?
https://github.com/STMicroelectronics/STM32DDRFW-UTIL?tab=readme-ov-file#222-add-local-aarch64-toolchain 

Did you tried to debug the code with CubeIDE ?
https://github.com/STMicroelectronics/STM32DDRFW-UTIL?tab=readme-ov-file#224-launch-project 


Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent