is there any way to find somewhere in memory address information about how many bytes I have written to FLASH memory on STM32H55
Hello ST community,
Is there a way to find information about how many bytes I've written to the flash memory of a certain memory area at some memory address (not starting at 0x0800000, but at 0x0802000)?
When I first power up, the byte counter is initialized to 0, and as I write bytes from address 0x0802000, I count the number of bytes, and at that point, I get the information about the number of bytes written.
But my goal is to know how many bytes I've previously written when I power cycle the STM32H7 MCU. Is there an option that counts the number of bytes written to the flash memory and automatically stores that information somewhere in the memory?
If so, which memory and at what address?
Thanks to anyone who can help me.
Regards