Skip to main content
Lead
Sep 10, 2024 11:38 PM UTC
Question

Is there any alternative Linux OS for the STM32MP1 system?

Hi!

I'm looking for an alternative Linux OS for the STM32MP1 system. I'm currently using OpenSTLinux, but it's very buggy and have a lack of lots of packages.

Can you recommend a Linux OS or that works with 512 MB Ram + 650 MHz CPU?

I'm planning to only replace the rootfs folder with the new linux distro.

This topic has been closed for replies.

2 replies

Macdog
Associate III
Sep 17, 2024 12:19 AM UTC

Several years back we ended up creating a Buildroot distribution, since then I believe that STMicro has offered official buildroot distributions for their ecosystem.    What packages are you looking for that are not available using Yocto or Buildroot?

 

DMårtAuthor
Lead
Sep 17, 2024 5:43 AM UTC

@Macdog 

I have created a Linux distro for stm32mp1 by using buiodroot.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer