Skip to main content
Associate II
Nov 25, 2024 1:06 PM UTC
Question

/initrd.image: incomplete write (-28 != 32769317)

Hello everyone,

I get an error when booting Linux + initramfs

The versions of the main components are:

Component

Version

tf-a-stm32mp

v2.6-stm32mp-r2.2

optee-os-stm32mp

v3.16.0-stm32mp-r2.2

u-boot-stm32mp

v2021.10-stm32mp-r2.2

linux-stm32mp

v5.15.145-stm32mp-r2.2

bootcmd:

 

setenv boot_device mmc;
setenv boot_instance 0;
setenv boot_partition 5;
setenv fit_addr C2000000;
mmc partactive ${boot_instance};
mmc partconf ${boot_device} 1 1 0;
load ${boot_device} ${boot_instance}:${boot_partition} ${fit_addr} fitImage-foo-image-initramfs;
setenv bootargs console=ttySTM0,115200 FIT_IMAGE_PART=${boot_partition} debug loglevel=8;
bootm ${fit_addr};

 

error:

 

[ 2.588644] rootfs image is not initramfs (write error); looks like an initrd
[ 2.588766] /initrd.image: incomplete write (-28 != 32769317)
[ 2.753422] Freeing initrd memory: 32004K

 

From my research I found that:

-28: ENOSPCwhich means No space left on device.

If I add: 

 

setenv initrd_high 0xFFFFFFFF

 

 

The error does not occur anymore. This is probably because the ramdisk is loaded directly from flash memory and not copied to RAM beforehand (see https://docs.u-boot.org/en/v2022.10/usage/environment.html)

The fitImage loading information states the following:

 

## Loading kernel from FIT Image at c2000000 ...
 Using 'conf-stm32mp151c-foo.dtb' configuration
 Trying 'kernel-1' kernel subimage
 Description: Linux kernel
 Created: 2023-12-23 9:42:00 UTC
 Type: Kernel Image
 Compression: uncompressed
 Data Start: 0xc2000120
 Data Size: 7437600 Bytes = 7.1 MiB
 Architecture: ARM
 OS: Linux
 Load Address: 0xc0800000
 Entry Point: 0xc0800000
 Hash algo: sha256
 Hash value: bf3e491301d2dc9fe63bf119ce4704a147f3dce0ca1168110ba7dd5b29e4cf63
 Verifying Hash Integrity ... sha256+ OK
## Loading ramdisk from FIT Image at c2000000 ...
 Using 'conf-stm32mp151c-foo.dtb' configuration
 Trying 'ramdisk-1' ramdisk subimage
 Description: foo-image-initramfs
 Created: 2023-12-23 9:42:00 UTC
 Type: RAMDisk Image
 Compression: uncompressed
 Data Start: 0xc2724e88
 Data Size: 32769317 Bytes = 31.3 MiB
 Architecture: ARM
 OS: Linux
 Load Address: unavailable
 Entry Point: unavailable
 Hash algo: sha256
 Hash value: 47c1724633530ff00903486d1bf7d334fa46c55ff7afedcb96b403c74c8c629f
 Verifying Hash Integrity ... sha256+ OK
## Loading fdt from FIT Image at c2000000 ...
Bootstage space exhasuted
Bootstage space exhasuted
 Using 'conf-stm32mp151c-foo.dtb' configuration
 Trying 'fdt-stm32mp151c-foo.dtb' fdt subimage
 Description: Flattened Device Tree blob
 Created: 2023-12-23 9:42:00 UTC
 Type: Flat Device Tree
 Compression: uncompressed
 Data Start: 0xc2717f54
 Data Size: 52840 Bytes = 51.6 KiB
 Architecture: ARM
 Hash algo: sha256
 Hash value: 1744a9700ebbe4faa2f35112ff30749cab8d769a205d082a970c65e72303f243
 Verifying Hash Integrity ... sha256+ OK
Bootstage space exhasuted
Bootstage space exhasuted
Bootstage space exhasuted
Bootstage space exhasuted
Bootstage space exhasuted
 Booting using the fdt blob at 0xc2717f54
 Loading Kernel Image
Bootstage space exhasuted
Bootstage space exhasuted
 Loading Ramdisk to c9fbb000, end cbefb525 ... OK
 Loading Device Tree to c9fab000, end c9fbae67 ... OK
Bootstage space exhasuted
Bootstage space exhasuted

Starting kernel ...

 

 

The ramdisk is successfully loaded into memory. But later on it can't be loaded into memory by the kernel?

The position c9fbb000 - cbefb525 is exactly the size of the initramfs 1F40525 = 32769317 bytes.

Compression of the initramfs

Has it something to do with the compression? Because the initramfs is in the format "cpio.gz" which means it is compressed with gzip. In the .its file (which is generated by yocto kernel-fitimage class) the compression is set to "none". If u-boot only allocates memory for the compressed initramfs and the kernel later on decompresses it and tries to load it into the same memory position it does not fit anymore maybe?

Any information on what is actually happening while this fitImage is booting would be appreciated.

 

 

 

This topic has been closed for replies.