Skip to main content
Associate III
Jan 25, 2024 5:02 AM UTC
Solved

Information regarding USBH from documentation

Hi

     I am working on a custom board based on STM32MP157A . For USBH_EHCI:

  • In USBH_EHCI_HCCPARAMS register there is a bit called "SFAC" is mentioned in reference manual(RM0436) .Could you please tell us what is the meaning and functionality of the bit.
  • In ehci-specification-for-usb(revision 1) the same bit is 64 - bit Addressing Capability

Register from reference manual :

USBH_EHCI.PNG

Register from ehci specification document :

HCCPARAMS.PNG

 

Regards

Srikanth

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
Jan 25, 2024 7:41 AM UTC

Hi @Srikanth1 

SFAC mean same than in EHCI documentation: "Sixty Four bits Addressing Capabilities".
As listed, it is at 0 in our implementation.

All USBH EHCI and OHCI registers in STM32MP1x fully comply with their relative specification as goal is to use standard available drivers (Linux or other operating system) which adapt their behavior to the read-only parameters provided.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

1 reply

PatrickF
PatrickFBest answer
ST Employee
Jan 25, 2024 7:41 AM UTC

Hi @Srikanth1 

SFAC mean same than in EHCI documentation: "Sixty Four bits Addressing Capabilities".
As listed, it is at 0 in our implementation.

All USBH EHCI and OHCI registers in STM32MP1x fully comply with their relative specification as goal is to use standard available drivers (Linux or other operating system) which adapt their behavior to the read-only parameters provided.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent