Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.
Most recent activity
Posted on June 25, 2017 at 21:18Hi !!!I am working on can-bus project with embedded linux environment. i tried porting linux on f4 discovery (f429) and the can bus pin wouldn't work on the machine some one said that i needed to cut C53 capacitor in order to use canbus . then i tried it on f407 discovery and canbus worked but i couldn't port linux on it. :(So Iam looking at two f7 discovery machine 1. stm32F746G DISCOVERY2. stm32F769I DISCOVERYCould anyone tell me if it is possible to port linux on stm32f7 discovery machine along with can bus pin enabled.if it is possible,which one should i choose ???thank you :)#embedded #stm32 #linux #can #canbus
Posted on May 26, 2017 at 16:25 Hello, I am having problems communicating with my NUCLEO-F767ZI board over the virtual COM port on Linux. The board uses USART3 to communicate via the ST-Link USB port with the PC. The ST-Link connects fine to the PC on device /dev/ttyACM0 and I can program it fine. I can even mount its disk partition as a mass storage device. I am using the re-routing of printf() to the USART interface to output debug text, as proposed in the ST examples, and this works fine on a Windows PC. On a Linux machine however, I don't get the output. I have tried 'screen' to open a serial console, as well as an Arduino IDE serial console, no luck. I have added udev rules for the ST-Link device in /etc/udev to be able to access the device without being root. I can work with other, Arduino-compatible boards over the same /dev/ttyACM0 device just fine. Does anyone have experience with these boards under Linux and can help me out? What am I missing here? #serial-interface #n
Posted on May 05, 2016 at 13:35It is a pity that ST hasn't released anything to program these memories under Linux, so I have developed a little utility to program STM32F7-discovery's QSPI Flash Memory.You can find it on my git repo:http://noosrequired.com/Javier_varez/QSPI_Programmer.gitI hope you find it useful. #stm32f7-discovery-kit #qspi #linux
Posted on May 18, 2015 at 19:25 IntoRobot, an experienced team of more than 20 faculty members and engineers, is going to release an open research platform, the Atom,by far the world's smallest open-source dual-CPU for IoTs and robotics. Following its motto �Let Atom be your private Engineer�, IntoRobot offers to help people who do not have a lot of knowledge about hardware, software or programming, to make their own complex IoT devices and robots; Atom is also designed to help people quickly build prototypes of their intelligent products. The cloud platform and all basic services are life-time free of charge. IntoRobot will launch Atom�s Kickstarter campaign SOON.The Atom,with the complex hardware and software details wrapped, is quite simple to operate through a friendly Web-interface. It allows you to connect devices in your dayly life, such as your flowerpot, aquarium,door, sockets, or induction cooker to the Internet very easily. You can
Posted on February 26, 2015 at 07:12is stm32 c compiler linux compatible? thank you regards kj #stm32 #linux
Posted on August 21, 2013 at 12:07Dear forum members please help me.... I want to programme my STM32F3 Discovery board using external St-link v2 programmer ,which pin of programmer should i connect with stm32f3 board. Thank you in advance. I know that stm32f3 has built in programmer ,but i don't want to use them for some reason... #stm32 #stm32 #linux #linux #debugger #debugging #debugging #debug-stm32-using-st-link/v2 #stm32-discovery
Posted on August 13, 2013 at 11:22Hi,I'm new to the STM3220G-Eval board and want to run uClinux on it. Are there any ready to use vendor files for uClinux like Makefile, config.arch, config.uClibc, config.linux-2.4 and so on? Or is there a similar controller which can be modified for the STM32F207?Has someone experience with uClinux on a STM32F2 controller? Thanks in advance for every kind of help.Kind regardsTido #stm32 #linux
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.