Skip to main content
Lead
Aug 11, 2024 9:35 PM UTC
Solved

I/TC: Primary CPU switching to normal world boot - I/TC: Forced system reset PSCI - Restarting from the beginning

I'm facing the issue were the USB connection is re-connecting, which results that STM32CubeProgrammer re-flashing the device over and over again when the fip-boot has be fully loaded. 

So what can cause this restarting and re-connection? Is it something with U-boot?

I have heard that CubeProgrammer may having some issues with timeouts, but in this case, the board is just restarting itself. FAQ : STM32MP1 STM32CubeProgrammer USB reconnect e... - STMicroelectronics Community

Here is the flashlayout:

 

#Opt	Id	Name	Type	IP	Offset	Binary
- 	0x01 	fsbl-boot 	Binary 	none 	0x0 	arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-usb.stm32
- 	0x03 	fip-boot 	FIP 	none 	0x0 	fip/fip-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.bin
P 	0x04 	fsbl1 	Binary 	mmc1 	boot1 	arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
P 	0x05 	fsbl2 	Binary 	mmc1 	boot2 	arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
P 	0x06 	metadata1 	FWU_MDATA 	mmc1 	0x00080000 	arm-trusted-firmware/metadata.bin
P 	0x07 	metadata2 	FWU_MDATA 	mmc1 	0x00100000 	arm-trusted-firmware/metadata.bin
P 	0x08 	fip-a 	FIP 	mmc1 	0x00180000 	fip/fip-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.bin
PED	0x09	fip-b 	FIP 	mmc1 	0x00580000 	none
PED	0x0A	u-boot-env 	ENV	mmc1 	0x00980000 	none
P 	0x10 	bootfs 	System 	mmc1 	0x00A00000 	st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P 	0x11 	vendorfs	FileSystem	mmc1 	0x04A00000 	st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P 	0x12 	rootfs 	FileSystem 	mmc1 	0x05A00000 	st-image-weston-openstlinux-weston-stm32mp1.ext4
P 	0x13 	userfs 	FileSystem 	mmc1 	0x33A00000 	st-image-userfs-openstlinux-weston-stm32mp1.ext4

 

Here is the last part of the log:

 

I/TC: DTB enables console (non-secure)
D/TC:0 0 call_initcalls:40 level 5 stm32mp_syscfg_enable_io_compensation()
D/TC:0 0 call_initcalls:40 level 5 init_pm_support()
D/TC:0 0 call_initcalls:40 level 5 probe_dt_drivers()
D/TC:0 0 stm32_tamp_parse_passive_conf:1608 Passive conf from dt: precharge=0, nb_sample=4, clk_div=16384
D/TC:0 0 stm32_tamp_parse_active_conf:1823 Active conf from dt: no filter clk_div=1
D/TC:0 0 gic_it_set_cpu_mask:350 cpu_mask: writing 0xff00 to 0xd86218e4
D/TC:0 0 gic_it_set_cpu_mask:352 cpu_mask: 0x300
D/TC:0 0 gic_it_set_prio:361 prio: writing 0x1 to 0xd86214e5
D/TC:0 0 add_node_to_probe:641 element: stm32_tamp_nvram on node nvram@5c00a100
D/TC:0 0 probe_driver_node:443 element: stm32-tamp on node tamp@5c00a000 initialized
D/TC:0 0 probe_driver_node:443 element: stm32_tamp_nvram on node nvram@5c00a100 initialized
D/TC:0 0 call_initcalls:40 level 6 init_stm32mp1_drivers()
D/TC:0 0 gic_it_set_cpu_mask:350 cpu_mask: writing 0x101ff01 to 0xd8621808
D/TC:0 0 gic_it_set_cpu_mask:352 cpu_mask: 0x1010101
D/TC:0 0 gic_it_set_prio:361 prio: writing 0x1 to 0xd8621409
D/TC:0 0 call_initcalls:40 level 6 stm32mp1_init_scmi_server()
D/TC:0 0 call_initcalls:40 level 6 stm32mp1_init_final_shres()
D/TC:0 0 stm32mp1_init_final_shres:438 stm32mp IWDG1 ( 0): unregistered 
D/TC:0 0 stm32mp1_init_final_shres:438 stm32mp USART1 ( 1): unregistered 
D/TC:0 0 stm32mp1_init_final_shres:438 stm32mp SPI6 ( 2): unregistered 
D/TC:0 0 stm32mp1_init_final_shres:438 stm32mp I2C4 ( 3): non-secure 
D/TC:0 0 stm32mp1_init_final_shres:438 stm32mp RNG1 ( 4): unregistered 
D/TC:0 0 stm32mp1_init_final_shres:438 stm32mp HASH1 ( 5): unregistered 
D/TC:0 0 stm32mp1_init_final_shres:438 stm32mp CRYP1 ( 6): unregistered 
D/TC:0 0 stm32mp1_init_final_shres:438 stm32mp I2C6 ( 7): unregistered 
D/TC:0 0 stm32mp1_init_final_shres:438 stm32mp RTC ( 8): unregistered 
D/TC:0 0 stm32mp1_init_final_shres:438 stm32mp MCU ( 9): unregistered 
D/TC:0 0 stm32mp1_init_final_shres:438 stm32mp PLL3 (10): unregistered 
D/TC:0 0 stm32mp1_init_final_shres:438 stm32mp MDMA (11): unregistered 
D/TC:0 0 stm32_bsec_find_otp_in_nvmem_layout:644 nvmem cfg0_otp = 0: 0 bit offset: 0, length: 8
D/TC:0 0 check_rcc_secure_configuration:347 RCC/PWR secure hardening: TZEN enable, MCKPROT enable
D/TC:0 0 call_initcalls:40 level 6 stm32mp_syscfg_set_hslv()
D/TC:0 0 stm32_bsec_find_otp_in_nvmem_layout:644 nvmem hw2_otp = 6: 18 bit offset: 0, length: 32
D/TC:0 0 call_initcalls:40 level 6 init_low_power()
D/TC:0 0 gic_it_set_cpu_mask:350 cpu_mask: writing 0xff00 to 0xd86218b0
D/TC:0 0 gic_it_set_cpu_mask:352 cpu_mask: 0x300
D/TC:0 0 gic_it_set_prio:361 prio: writing 0x1 to 0xd86214b1
D/TC:0 0 call_initcalls:40 level 6 stm32mp1_init_lp_states()
D/TC:0 0 stm32mp1_init_lp_states:230 Power configuration: shutdown to 6, suspend to 2
D/TC:0 0 call_initcalls:40 level 6 regulator_core_init()
D/TC:0 0 call_initcalls:40 level 7 stm32_rng_release()
D/TC:0 0 call_initcalls:40 level 7 regulator_core_cleanup()
D/TC:0 0 regulator_core_cleanup:916 disable usb33
D/TC:0 0 regulator_core_cleanup:916 disable reg18
D/TC:0 0 regulator_core_cleanup:916 disable reg11
D/TC:0 0 call_initcalls:40 level 7 release_probe_lists()
D/TC:0 0 call_finalcalls:59 level 1 release_external_dt()
I/TC: Primary CPU switching to normal world boot
I/TC: Forced system reset PSCI
NOTICE: CPU: STM32MP151AAC Rev.Z
NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mpu-v24.06.26
INFO: PMIC version = 0x21
WARNING: VDD unknown
INFO: Reset reason (0x54):
INFO: System reset generated by MPU (MPSYSRST)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: FCONF: Reading firmware configuration information for: stm32mp_fuse
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.8-stm32mp1-r2.0(debug):fc5a7b038-dirty(fc5a7b03)
NOTICE: BL2: Built : 23:46:56, Aug 6 2024
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
INFO: Memory size = 0x20000000 (512 MB)
INFO: DFU USB START...
INFO: phase ID :3, Manifestation 3 at c71615b2
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x2ffff000
INFO: Image id=1 loaded: 0x2ffff000 - 0x2ffff1ea
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0xde000000
INFO: Image id=4 loaded: 0xde000000 - 0xde00001c
INFO: OPTEE ep=0xde000000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0

 

 

The full log: https://pastebin.com/7JWA3eEG 

Here is the schematic of the USB. I'm using USB Micro.

Skärmklipp.PNG

This is the configuration of the USB-OTG for U-boot.

 

 

&usbotg_hs{
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&usb_otg_hs_pins_mx>;
	pinctrl-1 = <&usb_otg_hs_sleep_pins_mx>;
	status = "okay";

	/* USER CODE BEGIN usbotg_hs */
	/* This board does not have any USB-C connector */
	/* USER CODE END usbotg_hs */
};

 

 

Full configuration here: Configuration U-Boot 

Best regards

This topic has been closed for replies.
DMårtBest answer
Lead
Aug 12, 2024 4:43 PM UTC

Here is the solution. Then it boots into U-boot.

alias {
 serial0 = &uart4;
};

  

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer

1 reply

DMårtAuthorBest answer
Lead
Aug 12, 2024 4:43 PM UTC

Here is the solution. Then it boots into U-boot.

alias {
 serial0 = &uart4;
};

  

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer