Skip to main content
Lead
Aug 1, 2024 3:43 PM UTC
Solved

I got PANIC at PC : 0x2ffec98b - Why?

I made a custom board with the processor STM32MP151AAC3 and own firmwire https://github.com/DanielMartensson/STM32-Computer/tree/main/STM32CubeIDE/STM32-Computer-Firmware . I have compiled the TF-A by using STM32CubeIDE. It was some bugs with the TF-A configuration, but it seems I fixed them in this thread: 

Solved: BUG: Label or path X_pins_y not found - Compiling ... - STMicroelectronics Community

 

PANIC at PC : 0x2ffec98b

Exception mode=0x00000016 at: 0x2ffec98b

 

I have tried to flash it with firmware of STM32MP157 with another I2C4 pin configuration. And it failed. 

 

NOTICE: CPU: STM32MP151AAC Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157A eval daughter on eval mother
ERROR: I2C device not ready
PANIC at PC : 0x2fff101b

Exception mode=0x00000016 at: 0x2fff101b

Trying the Flashout Delete All DK1 STM32MP157a.
Exception mode=0x00000016 at: 0x2fff101b

NOTICE: CPU: STM32MP151AAC Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157A-DK1 Discovery Board
ERROR: I2C device not ready
PANIC at PC : 0x2fff101b

 

That means the following:

  1. The HSE clock is working
  2. The HSE clock is soldered correctly
  3. The I2C is working, even if it was not ready for communication (wrong pins)

Question:

This new error must lead to an answer. What can it be?

 

 

 

This topic has been closed for replies.
DMårtBest answer
Lead
Aug 4, 2024 8:18 PM UTC

@PatrickF 

I found the solution! The solution is this.

 

Add this to your stm32mp15xx-<project name->-mx.dts inside the tf-a device tree.

 

/* USER CODE BEGIN includes */
#include "stm32mp15xx-dkx.dtsi"
#include "stm32mp15-pinctrl.dtsi"
/* USER CODE END includes */

 

and this

 

	/* USER CODE BEGIN root */
	
	aliases {
		serial0 = &uart4;
	};

	chosen {
		stdout-path = "serial0:115200n8";
	};
	/* USER CODE END root */

 

 

 

	clocks {
		/* USER CODE BEGIN clocks */
		clk_hsi: clk-hsi {
			clock-frequency = <64000000>;

			/* USER CODE BEGIN clk_hsi */
			/* USER CODE END clk_hsi */
		};
		clk_lse: clk-lse {
			clock-frequency = <32768>;
			st,drive = < LSEDRV_MEDIUM_HIGH >;

			/* USER CODE BEGIN clk_lse */
			/* USER CODE END clk_lse */
		};
		clk_hse: clk-hse {
			clock-frequency = <24000000>;
			st,digbypass;

			/* USER CODE BEGIN clk_hse */
			/* USER CODE END clk_hse */
		};
		/* USER CODE END clocks */
	};

 

Last thing is to add cpu1 inside the stm32mp151.dtsi file in the fdts folder inside tf-a folder. Or else, you get one error when you're compiling.

 

	cpus {
		#address-cells = <1>;
		#size-cells = <0>;

		cpu0: cpu@0 {
			compatible = "arm,cortex-a7";
			device_type = "cpu";
			reg = <0>;
			nvmem-cells = <&part_number_otp>;
			nvmem-cell-names = "part_number";
		};
		
		cpu1: cpu@1 {
			/* EMPTY */
		};
	};

 

 Anyway!

With my FlashLayout, I only run to Id = 0x8 because I haven't done any more.

 

#Opt	Id	Name	Type	IP	Offset	Binary
-	0x01	fsbl-boot	Binary	none	0x0	arm-trusted-firmware/debug/debug-tf-a-stm32mp151a-stm32-computer-firmware-mx-usb.stm32
-	0x03	fip-boot	FIP	none	0x0	fip/fip-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.bin
P	0x04	fsbl1	Binary	mmc2	boot1	arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
P	0x05	fsbl2	Binary	mmc2	boot2	arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
P	0x06	metadata1	FWU_MDATA	mmc1	0x00080000	arm-trusted-firmware/metadata.bin
P	0x07	metadata2	FWU_MDATA	mmc1	0x00100000	arm-trusted-firmware/metadata.bin
P	0x08	fip-a	FIP	mmc2	0x00180000	fip/fip-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.bin
PED	0x09	fip-b	FIP	mmc2	0x00580000	none
PED	0x0A	u-boot-env	ENV	mmc1	0x00980000	none
P	0x10	bootfs	System	mmc1	0x00A00000	st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P	0x11	vendorfs	FileSystem	mmc1	0x04A00000	st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P	0x12	rootfs	FileSystem	mmc1	0x05A00000	st-image-weston-openstlinux-weston-stm32mp1.ext4
P	0x13	userfs	FileSystem	mmc1	0xC5A00000	st-image-userfs-openstlinux-weston-stm32mp1.ext4

 

This is the UART output. It seems that 

  • I started the SYSRAM
  • My STM32MP151AAC3 can communicate with my PMIC.

I think that the memory configuration is not correct, because I have 4GB RAM.

NOTICE: CPU: STM32MP151AAC Rev.Z
NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mpu-v24.06.26
INFO: PMIC version = 0x21
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: FCONF: Reading firmware configuration information for: stm32mp_fuse
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.8-stm32mp1-r2.0(debug):9b8d7c5be-dirty(9b8d7c5b)
NOTICE: BL2: Built : 20:53:22, Aug 3 2024
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
INFO: Memory size = 0x20000000 (512 MB)
INFO: DFU USB START...
INFO: phase ID :3, Manifestation 3 at c714f9a2
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x2ffff000
INFO: Image id=1 loaded: 0x2ffff000 - 0x2ffff1ea
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0xde000000
INFO: Image id=4 loaded: 0xde000000 - 0xde00001c
INFO: OPTEE ep=0xde000000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x1
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0xde000000
INFO: Image id=8 loaded: 0xde000000 - 0xde028e08
INFO: BL2: Skip loading image id 9
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0xc0500000
INFO: Image id=2 loaded: 0xc0500000 - 0xc0511bd8
INFO: BL2: Skip loading image id 16
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc0214c94
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0xde000000
INFO: SPSR = 0x1d3
I/TC: Early console on UART#4
I/TC: 
I/TC: Embedded DTB found
I/TC: OP-TEE version: f8cb4e8d8-dev (gcc version 12.3.0 (GCC)) #5 Sat Aug 3 23:25:35 UTC 2024 arm
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: Platform stm32mp1: flavor PLATFORM_FLAVOR - DT stm32mp151a-stm32-computer-firmware-mx.dts
I/TC: OP-TEE ST profile: system_services
E/TC:0 0 probe_dt_drivers:795 Probe sequence result: 0x80000000
E/TC:0 0 Panic

Conclusion:

I think I have answered my own question.

The problem was that SYSRAM did not start. But now it seems that I have made progress. 

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer

33 replies

PatrickF
ST Employee
Aug 1, 2024 4:14 PM UTC

Hi,

please clarify how did you get this message ? Boot from flash or download from CubeProgrammer ?

 

Few tips (maybe already covered):

- check if HSE setting (digital clock (bypass) or crystal oscillator) is aligned between HW (e.g. OSC_OUT) and TF-A Device Tree.
   e.g. if you are using a crystal, the st,digbypass should not be present in the DT
https://github.com/STMicroelectronics/arm-trusted-firmware/blob/v2.8-stm32mp/docs/devicetree/bindings/clock/st,stm32mp13-rcc.txt#L409

 

- Check (with an oscilloscope) if there is I2C correct transactions on the STPMIC1 pins

- Check what function could be related around address 0x2ffec98b in your compiled code.

- add more debugging messages

See also https://wiki.st.com/stm32mpu/wiki/How_to_debug_TF-A_BL2

Regards,

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
DMårtAuthor
Lead
Aug 1, 2024 5:22 PM UTC

Hi @PatrickF 

>> please clarify how did you get this message ? Boot from flash or download from CubeProgrammer ?

I got the message from UART via Arduino Monitor. I downloaded TF-A from CubeProgrammer.

 

>> - check if HSE setting (digital clock (bypass) or crystal oscillator) is aligned between HW (e.g. OSC_OUT) and TF-A Device Tree.
   e.g. if you are using a crystal, the st,digbypass should not be present in the DT

 

Yes. I have chosen Digital Pass and "st,digbypass" is present due to my 24 MHz Oscillator (not crystal).

STM32-Computer/STM32CubeIDE/STM32-Computer-Firmware/CA7/DeviceTree/STM32-Computer-Firmware/tf-a/stm32mp151a-stm32-computer-firmware-mx.dts at main · DanielMartensson/STM32-Computer (github.com)

 

>> - Check (with an oscilloscope) if there is I2C correct transactions on the STPMIC1 pins

It must be. I mean, it seems to be soldered correctly.

>> - Check what function could be related around address 0x2ffec98b in your compiled code.

How can I do that? 

Update:

I re-configure all the clocks to make sure that I did not miss anything.

Still got the same error code:

 

 19:27:23 : STM32CubeProgrammer API v2.17.0 | Windows-64Bits 
 19:28:25 : Read TSV File: C:\Users\danie\Downloads\en.FLASH-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26\stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26\images\stm32mp1\flashlayout_st-image-weston\optee\FlashLyout_STM32_Computer-Firmware.tsv
 19:28:25 : Number of partitions: 13
 19:29:20 : UR connection mode is defined with the HWrst reset mode
 19:29:21 : USB speed : High Speed (480MBit/s)
 19:29:21 : Manuf. ID : STMicroelectronics
 19:29:21 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
 19:29:21 : SN : 002600373431510433383938
 19:29:21 : DFU protocol: 1.1
 19:29:21 : Board : --
 19:29:21 : Device ID : 0x0500
 19:29:27 : Start Embedded Flashing service
 19:29:27 : Memory Programming ...
 19:29:27 : Opening and parsing file: tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
 19:29:27 : File : tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
 19:29:27 : Size : 224.44 KB 
 19:29:27 : Partition ID : 0x01 
 19:29:27 : Download in Progress:
 19:29:30 : File download complete
 19:29:30 : Time elapsed during download operation: 00:00:02.536
 19:29:30 : RUNNING Program ... 
 19:29:30 : PartID: :0x01 

----------------------------
PANIC at PC : 0x2ffec98b

Exception mode=0x00000016 at: 0x2ffec98b

 

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
DMårtAuthor
Lead
Aug 2, 2024 12:26 PM UTC

Hi @PatrickF 

I tried to change the clocks, without success. 

I tried to change the clocks so they will be exactly the same as these ones: STM32MP15 clock tree - stm32mpu

Then I generated the TF-A meta with stm32mp-stm32-computer-mx.stm32 file. I ONLY flashing the stm32mp-stm32-computer-mx.stm32 and not the fip/bin file.

I get the exactly the same issue:

 

 

PANIC at PC : 0x2ffec98b
Exception mode=0x00000016 at: 0x2ffec98b

 

 

But then I tried to use a pre-made FlashLayout FlashLayout_emmc_stm32mp157c-ed1-optee.tsv with CubeProgrammer. Then I got the classical issue that my I2C4 have wrong pinouts.

 

 

NOTICE: CPU: STM32MP151AAC Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157C eval daughter on eval mother
ERROR: I2C device not ready
PANIC at PC : 0x2fff101b

Exception mode=0x00000016 at: 0x2fff101b

 

 

 So that means:

  • The clocks is working
  • The soldering is working
  • No physical damage on the board

So my next question is: If I get the error 0x2ffec98b....and it's not the clocks. Perhaps you could send me the .ioc configuration file for STM32MP157x so I can copy over the most necessary parts to STM32MP151? I mean, it quite obvious that I have forgot something in the .ioc configuration. 

 

Update:

Do you think this has caused the problem: Solved: BUG: Label or path X_pins_y not found - Compiling ... - STMicroelectronics Community

I just changed the stm32mp15-bl2.dtsi file because the pins could not be found.

 
 
 
 
STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
PatrickF
ST Employee
Aug 2, 2024 1:27 PM UTC

Hi @DMårt 

ST boards .ioc configuration could obtained by just loading an STM32MP157x board (EV1 or DK1/2) in CubeMX. But it might not bring so much.

PatrickF_0-1722605034229.png

 

PatrickF_1-1722605096400.png

 

PatrickF_2-1722605114321.png

 

 

For ST boards .dts, please have a look to this folder https://github.com/STMicroelectronics/arm-trusted-firmware/tree/v2.8-stm32mp/fdts (see  also https://wiki.st.com/stm32mpu/wiki/STM32_MPU_device_tree#STM32MP1_series)

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
DMårtAuthor
Lead
Aug 2, 2024 2:19 PM UTC

Hi @PatrickF 

I have looked at stm32mp15-bl2.dtsi and it seems that there are some errors there.

If I comment the /omit-if-no-ref/, then the error disapear. But I might think that will cause the issue that my clocks wont start.

If I don't comment the /omit-if-no-ref/ then I will get the error "Label or path not found", because my pins are named e.g "i2c2_pins_mx" and not "i2c2_pins_a".

I think the ending "_mx" is the issue here. What do you think?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
DMårtAuthor
Lead
Aug 4, 2024 11:19 AM UTC

@PatrickF 

I have made one change. First, I did not use tf-a-usb.stm32 for fsbl-boot. Instead I was using tf-a-stm32mp151a-<projet name>-mx-optee-emmc.stm32 or tf-a-stm32mp151a-<project name>-mx-optee-sdcard.stm32. Which gave the same error code: 0x2ffec98b

 

But now I'm using tf-a-stm32mp151a-<project name>-mx-usb.stm32 for fsbl-boot and I got this error code now:

 

 

 

PANIC at PC : 0x2ffead5d

Exception mode=0x00000016 at: 0x2ffead5d

 

 

The memory map of ARM Trusted Firmware: 6.34. STMicroelectronics STM32MP1 — Trusted Firmware-A documentation

So that means that It's somthing with Bootloader 2 (BL2). 

0x00000000 +-----------------+
 | | ROM
0x00020000 +-----------------+
 | |
 | ... |
 | |
0x2FFC0000 +-----------------+ \
 | BL32 DTB | |
0x2FFC5000 +-----------------+ |
 | BL32 | |
0x2FFDF000 +-----------------+ |
 | ... | |
0x2FFE3000 +-----------------+ |
 | BL2 DTB | | Embedded SRAM
0x2FFEA000 +-----------------+ |
 | BL2 | |
0x2FFFF000 +-----------------+ |
 | SCMI mailbox | |
0x30000000 +-----------------+ /
 | |
 | ... |
 | |
0x40000000 +-----------------+
 | |
 | | Devices
 | |
0xC0000000 +-----------------+ \
 | | |
0xC0100000 +-----------------+ |
 | BL33 | | Non-secure RAM (DDR)
 | ... | |
 | | |
0xFFFFFFFF +-----------------+ /

 

What I have done is to change the build artifact for tf-a sources. I have replaced ..=optee-sdcard with ..=optee-usb.

When I'm trying to build the stm32 meta <project name>-mx build artifact. I'm not sure if that's correct.

I have also change the clocks so they are 100% the same as the default initialization of the system clocks of STM32MP157F-DK1.

Notice:

In STM32CubeIDE, for U-boot and Linux, you need to manually configure the clocks by pasting them into the .dts file. Yes, it's a bug and I hope the dev team of STM32CubeIDE will solve that in next version 1.17.0.

Question:

Which build artifact for tf-a in order to implement it into the SYSRAM by changing BL2?

https://github.com/DanielMartensson/STM32-Computer/tree/main/Firmware/STM32-Computer-Firmware

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
DMårtAuthor
Lead
Aug 4, 2024 8:16 PM UTC

@PatrickF 

I found the solution! The solution is this.

 

Add this to your stm32mp15xx-<project name->-mx.dts inside the tf-a device tree.

/* USER CODE BEGIN includes */
#include "stm32mp15xx-dkx.dtsi"
#include "stm32mp15-pinctrl.dtsi"
/* USER CODE END includes */

and this

	/* USER CODE BEGIN root */
	
	aliases {
		serial0 = &uart4;
	};

	chosen {
		stdout-path = "serial0:115200n8";
	};
	/* USER CODE END root */

 

	clocks {
		/* USER CODE BEGIN clocks */
		clk_hsi: clk-hsi {
			clock-frequency = <64000000>;

			/* USER CODE BEGIN clk_hsi */
			/* USER CODE END clk_hsi */
		};
		clk_lse: clk-lse {
			clock-frequency = <32768>;
			st,drive = < LSEDRV_MEDIUM_HIGH >;

			/* USER CODE BEGIN clk_lse */
			/* USER CODE END clk_lse */
		};
		clk_hse: clk-hse {
			clock-frequency = <24000000>;
			st,digbypass;

			/* USER CODE BEGIN clk_hse */
			/* USER CODE END clk_hse */
		};
		/* USER CODE END clocks */
	};

Last thing is to add cpu1 inside the stm32mp151.dtsi file in the fdts folder inside tf-a folder. Or else, you get one error when you're compiling.

	cpus {
		#address-cells = <1>;
		#size-cells = <0>;

		cpu0: cpu@0 {
			compatible = "arm,cortex-a7";
			device_type = "cpu";
			reg = <0>;
			nvmem-cells = <&part_number_otp>;
			nvmem-cell-names = "part_number";
		};
		
		cpu1: cpu@1 {
			/* EMPTY */
		};
	};

 Anyway!

With my FlashLayout, I only run to Id = 0x8 because I haven't done any more.

#Opt	Id	Name	Type	IP	Offset	Binary
-	0x01	fsbl-boot	Binary	none	0x0	arm-trusted-firmware/debug/debug-tf-a-stm32mp151a-stm32-computer-firmware-mx-usb.stm32
-	0x03	fip-boot	FIP	none	0x0	fip/fip-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.bin
P	0x04	fsbl1	Binary	mmc2	boot1	arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
P	0x05	fsbl2	Binary	mmc2	boot2	arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
P	0x06	metadata1	FWU_MDATA	mmc1	0x00080000	arm-trusted-firmware/metadata.bin
P	0x07	metadata2	FWU_MDATA	mmc1	0x00100000	arm-trusted-firmware/metadata.bin
P	0x08	fip-a	FIP	mmc2	0x00180000	fip/fip-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.bin
PED	0x09	fip-b	FIP	mmc2	0x00580000	none
PED	0x0A	u-boot-env	ENV	mmc1	0x00980000	none
P	0x10	bootfs	System	mmc1	0x00A00000	st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P	0x11	vendorfs	FileSystem	mmc1	0x04A00000	st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P	0x12	rootfs	FileSystem	mmc1	0x05A00000	st-image-weston-openstlinux-weston-stm32mp1.ext4
P	0x13	userfs	FileSystem	mmc1	0xC5A00000	st-image-userfs-openstlinux-weston-stm32mp1.ext4

This is the UART output. It seems that 

  • I started the SYSRAM
  • My STM32MP151AAC3 can communicate with my PMIC.

I think that the memory configuration is not correct, because I have 4GB RAM.

NOTICE: CPU: STM32MP151AAC Rev.Z
NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mpu-v24.06.26
INFO: PMIC version = 0x21
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: FCONF: Reading firmware configuration information for: stm32mp_fuse
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.8-stm32mp1-r2.0(debug):9b8d7c5be-dirty(9b8d7c5b)
NOTICE: BL2: Built : 20:53:22, Aug 3 2024
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
INFO: Memory size = 0x20000000 (512 MB)
INFO: DFU USB START...
INFO: phase ID :3, Manifestation 3 at c714f9a2
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x2ffff000
INFO: Image id=1 loaded: 0x2ffff000 - 0x2ffff1ea
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0xde000000
INFO: Image id=4 loaded: 0xde000000 - 0xde00001c
INFO: OPTEE ep=0xde000000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x1
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0xde000000
INFO: Image id=8 loaded: 0xde000000 - 0xde028e08
INFO: BL2: Skip loading image id 9
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0xc0500000
INFO: Image id=2 loaded: 0xc0500000 - 0xc0511bd8
INFO: BL2: Skip loading image id 16
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc0214c94
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0xde000000
INFO: SPSR = 0x1d3
I/TC: Early console on UART#4
I/TC: 
I/TC: Embedded DTB found
I/TC: OP-TEE version: f8cb4e8d8-dev (gcc version 12.3.0 (GCC)) #5 Sat Aug 3 23:25:35 UTC 2024 arm
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: Platform stm32mp1: flavor PLATFORM_FLAVOR - DT stm32mp151a-stm32-computer-firmware-mx.dts
I/TC: OP-TEE ST profile: system_services
E/TC:0 0 probe_dt_drivers:795 Probe sequence result: 0x80000000
E/TC:0 0 Panic

 

Conclusion:

I think I have answered my own question.

The problem was that SYSRAM did not start. But now it seems that I have made progress. 

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
DMårtAuthorBest answer
Lead
Aug 4, 2024 8:18 PM UTC

@PatrickF 

I found the solution! The solution is this.

 

Add this to your stm32mp15xx-<project name->-mx.dts inside the tf-a device tree.

 

/* USER CODE BEGIN includes */
#include "stm32mp15xx-dkx.dtsi"
#include "stm32mp15-pinctrl.dtsi"
/* USER CODE END includes */

 

and this

 

	/* USER CODE BEGIN root */
	
	aliases {
		serial0 = &uart4;
	};

	chosen {
		stdout-path = "serial0:115200n8";
	};
	/* USER CODE END root */

 

 

 

	clocks {
		/* USER CODE BEGIN clocks */
		clk_hsi: clk-hsi {
			clock-frequency = <64000000>;

			/* USER CODE BEGIN clk_hsi */
			/* USER CODE END clk_hsi */
		};
		clk_lse: clk-lse {
			clock-frequency = <32768>;
			st,drive = < LSEDRV_MEDIUM_HIGH >;

			/* USER CODE BEGIN clk_lse */
			/* USER CODE END clk_lse */
		};
		clk_hse: clk-hse {
			clock-frequency = <24000000>;
			st,digbypass;

			/* USER CODE BEGIN clk_hse */
			/* USER CODE END clk_hse */
		};
		/* USER CODE END clocks */
	};

 

Last thing is to add cpu1 inside the stm32mp151.dtsi file in the fdts folder inside tf-a folder. Or else, you get one error when you're compiling.

 

	cpus {
		#address-cells = <1>;
		#size-cells = <0>;

		cpu0: cpu@0 {
			compatible = "arm,cortex-a7";
			device_type = "cpu";
			reg = <0>;
			nvmem-cells = <&part_number_otp>;
			nvmem-cell-names = "part_number";
		};
		
		cpu1: cpu@1 {
			/* EMPTY */
		};
	};

 

 Anyway!

With my FlashLayout, I only run to Id = 0x8 because I haven't done any more.

 

#Opt	Id	Name	Type	IP	Offset	Binary
-	0x01	fsbl-boot	Binary	none	0x0	arm-trusted-firmware/debug/debug-tf-a-stm32mp151a-stm32-computer-firmware-mx-usb.stm32
-	0x03	fip-boot	FIP	none	0x0	fip/fip-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.bin
P	0x04	fsbl1	Binary	mmc2	boot1	arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
P	0x05	fsbl2	Binary	mmc2	boot2	arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
P	0x06	metadata1	FWU_MDATA	mmc1	0x00080000	arm-trusted-firmware/metadata.bin
P	0x07	metadata2	FWU_MDATA	mmc1	0x00100000	arm-trusted-firmware/metadata.bin
P	0x08	fip-a	FIP	mmc2	0x00180000	fip/fip-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.bin
PED	0x09	fip-b	FIP	mmc2	0x00580000	none
PED	0x0A	u-boot-env	ENV	mmc1	0x00980000	none
P	0x10	bootfs	System	mmc1	0x00A00000	st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P	0x11	vendorfs	FileSystem	mmc1	0x04A00000	st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P	0x12	rootfs	FileSystem	mmc1	0x05A00000	st-image-weston-openstlinux-weston-stm32mp1.ext4
P	0x13	userfs	FileSystem	mmc1	0xC5A00000	st-image-userfs-openstlinux-weston-stm32mp1.ext4

 

This is the UART output. It seems that 

  • I started the SYSRAM
  • My STM32MP151AAC3 can communicate with my PMIC.

I think that the memory configuration is not correct, because I have 4GB RAM.

NOTICE: CPU: STM32MP151AAC Rev.Z
NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mpu-v24.06.26
INFO: PMIC version = 0x21
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: FCONF: Reading firmware configuration information for: stm32mp_fuse
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.8-stm32mp1-r2.0(debug):9b8d7c5be-dirty(9b8d7c5b)
NOTICE: BL2: Built : 20:53:22, Aug 3 2024
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
INFO: Memory size = 0x20000000 (512 MB)
INFO: DFU USB START...
INFO: phase ID :3, Manifestation 3 at c714f9a2
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x2ffff000
INFO: Image id=1 loaded: 0x2ffff000 - 0x2ffff1ea
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0xde000000
INFO: Image id=4 loaded: 0xde000000 - 0xde00001c
INFO: OPTEE ep=0xde000000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x1
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0xde000000
INFO: Image id=8 loaded: 0xde000000 - 0xde028e08
INFO: BL2: Skip loading image id 9
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0xc0500000
INFO: Image id=2 loaded: 0xc0500000 - 0xc0511bd8
INFO: BL2: Skip loading image id 16
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc0214c94
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0xde000000
INFO: SPSR = 0x1d3
I/TC: Early console on UART#4
I/TC: 
I/TC: Embedded DTB found
I/TC: OP-TEE version: f8cb4e8d8-dev (gcc version 12.3.0 (GCC)) #5 Sat Aug 3 23:25:35 UTC 2024 arm
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: Platform stm32mp1: flavor PLATFORM_FLAVOR - DT stm32mp151a-stm32-computer-firmware-mx.dts
I/TC: OP-TEE ST profile: system_services
E/TC:0 0 probe_dt_drivers:795 Probe sequence result: 0x80000000
E/TC:0 0 Panic

Conclusion:

I think I have answered my own question.

The problem was that SYSRAM did not start. But now it seems that I have made progress. 

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
Associate II
Sep 11, 2024 12:43 PM UTC

Hi @DMårt 

Have you moved forward with your board running process? I am in exactly the same place as your log snip shows. I have the following output:

I/TC: OP-TEE ST profile: system_services
E/TC:0 0 probe_dt_drivers:795 Probe sequence result: 0x80000000
E/TC:0 0 Panic

 

DMårtAuthor
Lead
Sep 11, 2024 12:54 PM UTC

@rgruberski 

Do you have the same processor as In do?

If yes, check your my custom board. It's working like a charm!

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer