Skip to main content
Associate II
Feb 4, 2026 12:32 PM UTC
Question

HSEM registers access has except on STM32MP257 in development mode

I have used HSEM on STM32H7 very well.

Recently,I test the HSEM of STM32MP257 in development mode, by JTAG/SWD,
I can lock the semaphore by reading the HSEM_RLRx register via CPU1~3,

but after power reset,when I write the HSEM_RLRx register to lock or unlock semaphore, it doesn't work!
the security /privilege / CID filtering of HSEM are all off after reset, and the cpu3 could  access the HSEM_RLRx register correctly,but after cpu1/2  write the HSEM_RLRx register or HSEM_CnIER,both lock and unlock operations have no effect.

pls give me some suggestions to check what I might have done wrong .thanks!

2 replies

Da_VinciAuthor
Associate II
Feb 6, 2026 12:15 PM UTC

And why the newest STM32MP21 series has deleted the HSEM module ?

This module is quite useful in multi-core applications.

PatrickF
ST Employee
Feb 6, 2026 4:24 PM UTC

As far as I know, HSEM is inherited from STM32MP15 family but finally not used in STM32MP25 and STM32MP23 software as all our inter-processor communication uses IPCC (also in STM32MP15).

I confirm it has been removed in STM32MP21.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent