Skip to main content
PDzie.1
Associate II
Jun 24, 2020 7:15 PM UTC
Question

How to run android on stm32mp157c-dk2

Hi,

I'm lead embedded engineer at some company. Our current tech stack is android board for GUI and networking connected to stm32f2 over uart, which controls our hardware.

We're trying to give a shot to stm32mp1, which could be great way to reduce hardware cost and give us better tools to offload some not-real-time, but cpu intensive, tasks to application processor.

We've bought STM32MP157C-DK2 with intention of porting our software on it. First step would, obviously, be running Android on it. Since we've got android image from vendor of our current android boards and modified it only slightly, we have no experience with android development. Where should we start? I assume that it should be rather simple task, since ST provides bsp for stm32mp157c-ev1; which shares same MPU. I basically need, right now, usb storage, MIPI DSI display (DK2's built in one will be fine for now) with touch screen and uart peripheral. I'll leave running wifi dongle, usb camera and ethernet for later.

This topic has been closed for replies.

7 replies

mleo
Visitor II
Jun 25, 2020 12:39 PM UTC

Hello @PDzie.1​ ,

Have you already visited android related st wiki?

It contains set of useful articles:

https://wiki.st.com/stm32mpu/wiki/Category:How_to_Android

I believe it make you progress

Best regards,

Milan

PDzie.1
PDzie.1Author
Associate II
Jun 25, 2020 2:33 PM UTC

Hi,

Thanks @mleo​ . I've read this wiki, but got stuck on Embedded Software page.

https://wiki.st.com/stm32mpu/wiki/How_to_create_your_own_STM32MPU_distribution_for_Android

I guess it's right place to start then. I've briefly looked at it and it seems thorough and I'm surely going to ask again when I got stuck.

Anyway, why did you prepare image for -ev1 only? -EV1 is much more expensive (4 times?) and was not available when I ordered -dk2 devkit.

Best regards,

Paweł

PatrickF
ST Employee
Jun 26, 2020 7:13 AM UTC

Hello,

EV1 benefit of 1GBytes 32-bit DDR whereas DK2 has only 512MBytes 16-bits DDR which make Android performance too low for a good user experience in most application. If you think your application might flight on DK2, you should have to built an image for the DK2.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
PDzie.1
PDzie.1Author
Associate II
Jun 30, 2020 1:22 PM UTC

Ok... I'm really close to getting started for real (now I just do research in short pauses between other tasks).

If I understand wiki page correctly, to build Android for -DK2 from ST's distribution I have to:

  1. Create new dir under device/stm/stm32mp1/, lets say /device/stm/stm32mp1/dk2 and copy content from eval.
  2. Modify device tree, can I just copy one from stm32mp157c-dk2 linux distro? Replace them in stm32mp1-xxxxxxx directories, or just copy new ones ( I guess makefiles and configs will point to right one, after setting everything up).
  3. Modify makefiles and overlay, as described in here: https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/How_to_create_your_own_STM32MPU_distribution_for_Android#Create_your_device . Giving it a brief look, none of it seems very complicated.
  4. Flash layout should be OK, as long as I choose SDCard 8GB build variant?

That should be enough to create distribution for -DK2 board? I know that it would be just basic one, and would require a bit tuning, but that should just work (I mean, I should be able to run it on devkit and see something on it's display)? Seems a bit too easy.

Looking a bit further into the future, I could just get vendor's linux distribution, take device tree from there, do same things as with -dk2 and all should just work? Or generating my own from STM32CubeMX would be safer choice?

@edit

@PatrickF​ We will be fine if it will work with resolution up to 800x480 only :). That would be perhaps a bit problematic if we would like to upgrade to bigger displays, but even then there are plenty of 7" displays with 800x480 resolution.

VPete.1
Associate
Aug 31, 2020 3:24 PM UTC

Hello PDzie.1

did you succeed in building Android for the -DK2 in the described way?

Best

Volker.