Skip to main content
Associate II
May 27, 2025 3:06 AM UTC
Solved

How to modify metadata.bin file?

Hello

I am working on the multi-system in STM32MP257-EV board, I had modified the tsv file to prepare a double system A and B. If using the default metadata.bin file, the A system will be run always. Now I want the B system to be run, I need to modify the metadata.bin file, for example change the "accepted" of B bank to false:

longfeili_00001_0-1748314728273.png

If the status of img_0_bank_1 is trial, the B bank system will be run when ev board power up, isn't it?

how to modify the metadata.bin?

If the status of img_0_bank_1 has been modified to trial, and the B bank system run up normally, is the status of img_0_bank_1 modified automatically by linux? how does the linux system modify the metadata.bin file?

This topic has been closed for replies.
Christophe Guibout
ST Technical Moderator
May 27, 2025 7:08 AM UTC

Hi @longfeili_00001,

 

I written a wiki page which answers to your question, but it's not yet published.

I copy paste the content of the article:

 

How to update the metadata content?

The mkfwumdata tool (from U-Boot) is used to generate the metadata partition.

Metadata generation is described in the following wiki article: Metadata generation tool, nevertheless, this version of mkfwumdata doesn't support valid bank state (only accepted and invalid are supported).

So, please apply the following patch in U-Boot to bring the feature (this patch will be integrated in v6.1.0 Ecosystem Release): autoboot-propagate-boot-index.patch .

 

 

FWU states vs Firmware Update states

FWU metadata considers three states where two of them can correspond to Firmware update state machine:

 

Steps to run a FOTA update

  • Prerequisite: system is running on bank A (fip-a, bootfs-a, rootfs-a...)
  • The update manager which is in touch with the software provisioning server is notified about a new update that will be written into bank B (fip-b, bootfs-b, rootfs-b...)
  • When the new image is downloaded into the bank B, the update manager:
    • can execute some scripts to adapt the new flashed image to bank B (ex: partition mount points)
    • update the metadata partition to request TF-A to try to boot on the new bank B: so the update manager will change the metadata partition by:
      • updating active_index to bank B (see -a option), so bank A becomes previous_active_index (see -p option)
      • switching bank B as Valid (see -s option). Bank A will be kept as Accepted, in case of failure of bank B.

 

UUID_LIST="8a7a84a0-8387-40f6-ab41-a8b9a5a60d23,19d5df83-11b0-457b-be2c-7559c13142a5,4fd84c93-54ef-463f-a7ef-ae25ff887087,09c54952-d5bf-45af-acee-335303766fb3"

OPTIONS="-g -i 1 -b 2 -v 2"

bank_state="A,V"

mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata1

mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata2

 

 

Don't forget to update /dev/disk/by-partlabel/metadata2 which is the backup of metadata1, and will be used by TF-A in case of CRC error of metadata1 partition.

  • On reboot, TF-A will boot bank B, and we have now two possibilities:
    • bank B crashs: as the watchdog is enabled, the platform will reboot on crash. As bank B is in trial mode, the bootcount is decremented on each reboot. After 3 attempts (default value), TF-A will consider the bank B is not able to boot, so it will switch back to bank A. As active_index is bank B, but bank A is active, the update manager can consider bank B as Invalid, and notify the software provisioning server if needed.
    • bank B successfully boots: the update manager from bank B can update the metadata partition to switch the bank B state to Accepted: on the next reboot, TF-A will consider this bank Accepted, and will disable the bootcount:

UUID_LIST="8a7a84a0-8387-40f6-ab41-a8b9a5a60d23,19d5df83-11b0-457b-be2c-7559c13142a5,4fd84c93-54ef-463f-a7ef-ae25ff887087,09c54952-d5bf-45af-acee-335303766fb3"

OPTIONS="-g -i 1 -b 2 -v 2"

bank_state="A,A"

mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata1

mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata2

 

 

This can be done in a systemd service:

$ cat status-mark-good.service [Unit] Description=Good-marking Service [Service] ExecStart=/bin/bash /usr/bin/st-status-mark-good.sh [Install] WantedBy=multi-user.target

where st-status-mark-good.sh script asks the update manager to update the metadata partition to switch the bank B state to Accepted.

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

6 replies

Christophe Guibout
ST Technical Moderator
May 27, 2025 7:08 AM UTC

Hi @longfeili_00001,

 

I written a wiki page which answers to your question, but it's not yet published.

I copy paste the content of the article:

 

How to update the metadata content?

The mkfwumdata tool (from U-Boot) is used to generate the metadata partition.

Metadata generation is described in the following wiki article: Metadata generation tool, nevertheless, this version of mkfwumdata doesn't support valid bank state (only accepted and invalid are supported).

So, please apply the following patch in U-Boot to bring the feature (this patch will be integrated in v6.1.0 Ecosystem Release): autoboot-propagate-boot-index.patch .

 

 

FWU states vs Firmware Update states

FWU metadata considers three states where two of them can correspond to Firmware update state machine:

 

Steps to run a FOTA update

  • Prerequisite: system is running on bank A (fip-a, bootfs-a, rootfs-a...)
  • The update manager which is in touch with the software provisioning server is notified about a new update that will be written into bank B (fip-b, bootfs-b, rootfs-b...)
  • When the new image is downloaded into the bank B, the update manager:
    • can execute some scripts to adapt the new flashed image to bank B (ex: partition mount points)
    • update the metadata partition to request TF-A to try to boot on the new bank B: so the update manager will change the metadata partition by:
      • updating active_index to bank B (see -a option), so bank A becomes previous_active_index (see -p option)
      • switching bank B as Valid (see -s option). Bank A will be kept as Accepted, in case of failure of bank B.

 

UUID_LIST="8a7a84a0-8387-40f6-ab41-a8b9a5a60d23,19d5df83-11b0-457b-be2c-7559c13142a5,4fd84c93-54ef-463f-a7ef-ae25ff887087,09c54952-d5bf-45af-acee-335303766fb3"

OPTIONS="-g -i 1 -b 2 -v 2"

bank_state="A,V"

mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata1

mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata2

 

 

Don't forget to update /dev/disk/by-partlabel/metadata2 which is the backup of metadata1, and will be used by TF-A in case of CRC error of metadata1 partition.

  • On reboot, TF-A will boot bank B, and we have now two possibilities:
    • bank B crashs: as the watchdog is enabled, the platform will reboot on crash. As bank B is in trial mode, the bootcount is decremented on each reboot. After 3 attempts (default value), TF-A will consider the bank B is not able to boot, so it will switch back to bank A. As active_index is bank B, but bank A is active, the update manager can consider bank B as Invalid, and notify the software provisioning server if needed.
    • bank B successfully boots: the update manager from bank B can update the metadata partition to switch the bank B state to Accepted: on the next reboot, TF-A will consider this bank Accepted, and will disable the bootcount:

UUID_LIST="8a7a84a0-8387-40f6-ab41-a8b9a5a60d23,19d5df83-11b0-457b-be2c-7559c13142a5,4fd84c93-54ef-463f-a7ef-ae25ff887087,09c54952-d5bf-45af-acee-335303766fb3"

OPTIONS="-g -i 1 -b 2 -v 2"

bank_state="A,A"

mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata1

mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata2

 

 

This can be done in a systemd service:

$ cat status-mark-good.service [Unit] Description=Good-marking Service [Service] ExecStart=/bin/bash /usr/bin/st-status-mark-good.sh [Install] WantedBy=multi-user.target

where st-status-mark-good.sh script asks the update manager to update the metadata partition to switch the bank B state to Accepted.

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
May 27, 2025 11:32 AM UTC

Hello Christophe

Thanks for your reply!

I had add the patch into my uboot code and rebuilt the uboot, but no new mkfwumdata tool generated. The following is the command used to build the uboot:

make -f $PWD/../Makefile.sdk DEPLOYDIR=$FIP_DEPLOYDIR_ROOT/u-boot UBOOT_CONFIG="default programmer" UBOOT_DEFCONFIG=stm32mp25_defconfig UBOOT_BINARY=u-boot.dtb DEVICE_TREE=stm32mp257f-ev1 FIP_CONFIG="optee-sdcard optee-programmer-usb" all

can this command build out the new mkfwumdata tool? 

how does the mkfwumdata tool generated?

Christophe Guibout
ST Technical Moderator
May 27, 2025 12:05 PM UTC

In configs/stm32mp25/defconfig:

CONFIG_TOOLS_MKFWUMDATA=y

Then,

make stm32mp25_defconfig

make DEVICE_TREE=stm32mp257f-ev1 all -j12

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
May 27, 2025 12:37 PM UTC

hello Christophe

the new mkfwumdata tool has been generated:

./mkfwumdata --help
Usage: mkfwumdata [options] <UUIDs list> <output file>
Options:
-i, --images <num> Number of images (mandatory)
-b, --banks <num> Number of banks (mandatory)
-v, --version Metadata version (mandatory)
-s, --bank-state <val> list of bank states (default=A (accepted), V(valid) or I(invalid)
-a, --active-bank <num> Active bank (default=0)
-p, --previous-bank <num> Previous active bank (default=active_bank - 1)
-g, --guid Use GUID instead of UUID
-V, --vendor-file Vendor data file to append to the metadata
-h, --help print a help message


And regenerate the metadata.bin file use the following command:

./mkfwumdata -g -i 1 -b 2 -v 2 -s "A,V" -a 1 -p 0 8a7a84a0-8387-40f6-ab41-a8b9a5a60d23,19d5df83-11b0-457b-be2c-7559c13142a5,4fd84c93-54ef-463f-a7ef-ae25ff887087,09c54952-d5bf-45af-acee-335303766fb3 ~/metadata_tool/metadat
a.bin

Then, I use the fwumd_tool.py tool in tf-a transfer bin file to json file:

./fwumd_tool.py binparse ~/metadata_tool/metadata.bin -j ~/metadata_tool/metadata.json

Then, cat it to check if the status of bank changed or not, and it looks like the new tool not work:

cat ~/metadata_tool/metadata.json
{
"metadata": {
"crc_32": 3929930603,
"version": 2,
"active_index": 1,
"previous_active_index": 0,
"img_entry": {
"img_0": {
"location": "loc_00010002_0050_0018_83df_d519b0117b45",
"img_bank_info": {
"img_0_bank_0": {
"accepted": true,
"reserved": 588097189
},
"img_0_bank_1": {
"accepted": true,
"reserved": 0
}
}
}
}
},

 

Christophe Guibout
ST Technical Moderator
May 27, 2025 1:18 PM UTC

@longfeili_00001,

 

The tool named fwumd_tool.py is only compatible with metadata v1.

The tool named mkfwumdata is only compatible with metadata v2.

 

Here, you used fwumd_tool.py with metadata v2.

To check if the metadata is well built with mkfwumdata, write the generated file into metadata partitions, are reboot the platform to check the impact in TF-A.

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
May 28, 2025 2:21 AM UTC

Hello

Thanks very much, it looks work well.