Skip to main content
Associate II
Apr 8, 2025 3:43 AM UTC
Question

How to get complete Qt dependencies on STM32MP25?

I'm trying to get PySide6 and some common Python packages on my STM32MP257. "apt-get install python3-PySide6" doesn't work. I also tried to install the PySide6 package using pip3, which installed successfully, but gave me the error "ImportError: libX11.so.6: cannot open shared object file: No such file or directory" when I actually ran it. It seems to be missing some dependencies to support the Qt and GUI development I want to do. At this point, I'm stuck. I am using the STM32MP257F-DK development kit.

This topic has been closed for replies.

1 reply

PPAGE.13
ST Employee
Jul 1, 2025 7:15 AM UTC

Hi,

PySide6 is not part of the X-LINUX-QT Starter Package. There is no PySide6 debian package on our server. This is due to redistribution legal constraints.

 

You need to rebuild the Distribution to get the lib.

https://wiki.st.com/stm32mpu/wiki/X-LINUX-QT_Expansion_Package

And more specifically:

https://wiki.st.com/stm32mpu/wiki/X-LINUX-QT_Distribution_Package

with following recipe "python3-pyside6" to be added:

https://layers.openembedded.org/layerindex/recipe/380679/

 

BR,

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.