Skip to main content
Wjian.1
Associate III
Dec 15, 2020 2:44 AM UTC
Question

How to generate independently serialboot.stm32 file?

Hi:​

I encountered a strange problem when I compiled TF source code separately to generate xxserialboot.stm32 File, but found that there are always errors? ​eg:

make -f $PWD/../Makefile.sdk TFA_DEVICETREE=stm32mp157c-dk2 TF_A_CONFIG=serialboot ELF_DEBUG_ENABLE='1' all

​But complain about the compiler:

arm-ostl-linux-gnueabi-gcc: error: unrecognized command line option '-mstrict-align'; did you mean '-Wstrict-aliasing'?

But it's normal when I compile the trust file alone:

​make -f $PWD/../Makefile.sdk TFA_DEVICETREE=stm32mp157c-dk2 TF_A_CONFIG=trusted ELF_DEBUG_ENABLE='1' all

​How can I fix this problem?Could you give me some advice?

Best regards!​

​

​

​

​

This topic has been closed for replies.

1 reply

Bernard PUEL
ST Technical Moderator
Jan 25, 2021 4:59 PM UTC

Hello, if you are on V2.0.0 please see this post with the updated Makefile.sdk (there was on issue for serial target): https://community.st.com/s/question/0D53W00000HOJdOSAX/use-v22r0-tfa-to-burn-to-stm32mp157cev1-via-stm32programmercli-usb-is-not-supported

Or you can move to V2.1.0 that has also this correction. IF you follow the README file, there shouldn't be any issue.