Skip to main content
Associate II
Oct 4, 2025 9:36 AM UTC
Question

How to add a custom mode for HDMI display

I would like to add a custom resolution hdmi display (1024x600) to my STM32MP257F-DK  board  is it possible as the dmesg output is as follows 

[ 930.525408] [drm:drm_helper_probe_single_connector_modes] [CONNECTOR:32:HDMI-A-1]
[ 930.590130] stm32-display 48010000.display-controller: [drm:update_display_info.part.0] [CONNECTOR:32:HDMI-A-1] ELD monitor
[ 930.590170] stm32-display 48010000.display-controller: [drm:update_display_info.part.0] [CONNECTOR:32:HDMI-A-1] ELD size 20, SAD count 0
[ 930.590208] stm32-display 48010000.display-controller: [drm:update_display_info.part.0] [CONNECTOR:32:HDMI-A-1] ELD monitor
[ 930.590223] stm32-display 48010000.display-controller: [drm:update_display_info.part.0] [CONNECTOR:32:HDMI-A-1] ELD size 20, SAD count 0
[ 930.591397] [drm:drm_mode_debug_printmodeline] Modeline "1024x600": 60 49000 1024 1072 1168 1312 600 603 613 624 0x48 0xa
[ 930.591421] [drm:drm_mode_prune_invalid] Not using 1024x600 mode: CLOCK_RANGE
[ 930.591433] [drm:drm_mode_debug_printmodeline] Modeline "800x450": 60 27759 800 816 896 992 450 451 454 466 0x0 0x6
[ 930.591450] [drm:drm_mode_prune_invalid] Not using 800x450 mode: CLOCK_RANGE

The display shows CLOCK_RANGE, is there any possible way to add a custom resolution if it is not present by default in the edid data.

5 replies

Erwan SZYMANSKI
ST Technical Moderator
Oct 7, 2025 1:59 PM UTC

Hello @Samip_veer ,
Please can you take a look at this wiki article: https://wiki.st.com/stm32mpu/wiki/How_to_display_on_HDMI

I think it can highlight some points you are looking for.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
Oct 10, 2025 6:51 AM UTC

Dear @Erwan SZYMANSKI 

Thank you for your reply i had aldready studied the article and also checked various community discussion but the problem if CLOCK_RANGE means i need to set the clock frequency so that the pixel clock frequency matches with my device, can you help me with that as i did not find any relevant material in the article.

Erwan SZYMANSKI
ST Technical Moderator
Oct 13, 2025 7:01 AM UTC

Hi @Samip_veer ,
Did you already check this answer from Antonio ? https://community.st.com/t5/stm32-mpus-products-and-hardware/what-are-the-criteria-for-modetest-to-accept-a-modeline/td-p/268952

Did you try to activate debug too to get the exact clock value you get VS the one that is expected ?

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
Nov 25, 2025 10:23 AM UTC

Dear Erwan,

                          Sorry for the late reply yes, Yes i have debug the output as per the answer from Antonio and i get the below output:-

[ 214.829812] [drm:drm_helper_probe_single_connector_modes] [CONNECTOR:32:HDMI-A-1]
[ 214.894601] stm32-display 48010000.display-controller: [drm:update_display_info.part.0] [CONNECTOR:32:HDMI-A-1] ELD monitor
[ 214.894641] stm32-display 48010000.display-controller: [drm:update_display_info.part.0] [CONNECTOR:32:HDMI-A-1] ELD size 20, SAD count 0
[ 214.894673] stm32-display 48010000.display-controller: [drm:update_display_info.part.0] [CONNECTOR:32:HDMI-A-1] ELD monitor
[ 214.894688] stm32-display 48010000.display-controller: [drm:update_display_info.part.0] [CONNECTOR:32:HDMI-A-1] ELD size 20, SAD count 0
[ 214.895319] [drm:ltdc_encoder_mode_valid] clk rate target 49000000, available 49500000
[ 214.895868] [drm:ltdc_encoder_mode_valid] clk rate target 27759000, available 28285714
[ 214.895882] [drm:drm_mode_debug_printmodeline] Modeline "1024x600": 60 49000 1024 1072 1168 1312 600 603 613 624 0x48 0xa
[ 214.895903] [drm:drm_mode_prune_invalid] Not using 1024x600 mode: CLOCK_RANGE
[ 214.895914] [drm:drm_mode_debug_printmodeline] Modeline "800x450": 60 27759 800 816 896 992 450 451 454 466 0x0 0x6
[ 214.895931] [drm:drm_mode_prune_invalid] Not using 800x450 mode: CLOCK_RANGE

There is a difference in the clock range, How can i solve this problem please advice. I intent to use the 1024x600 resolution for this purpose.

 

Regards,

Samip

 

 

Associate II
Dec 6, 2025 7:27 AM UTC

Hey @Erwan SZYMANSKI  can you help me on this ? or is it not possible to attach this display?