Skip to main content
KAlab.1
Visitor II
Aug 16, 2020 7:42 PM UTC
Question

How do I interface mipi dsi 2-lane with 4-lane displays?

I cannot find compatible displays for this processor.

This topic has been closed for replies.

4 replies

AntonioST
ST Employee
Aug 16, 2020 7:58 PM UTC

Usually display panels can be configured for the amount of DSI lanes that would be used.

The number of lanes should be specified as one of the properties in the devicetree.

But check carefully while selecting the display. For example, this one only accepts 3 or 4 as value for the property 'dsi-lanes'

https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git/tree/Documentation/devicetree/bindings/display/panel/raydium,rm67191.yaml#n25

Tesla DeLorean
Guru
Aug 16, 2020 8:31 PM UTC

Two lanes a bit design limiting in a world expecting FHD and UHD displays..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AntonioST
ST Employee
Aug 16, 2020 8:55 PM UTC

The datasheet reports:

> LCD-TFT controller, up to 24-bit // RGB888

> – up to WXGA (1366 × 768) @60 fps

Tesla DeLorean
Guru
Aug 16, 2020 8:30 PM UTC

Configure the display controller..

Two lanes will limit the total resolution, colour depth and refresh rate.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..