FWU rollback counter is not reset (after rauc-mark-good) on consecutive updates in FWU
- 8 replies
- 1208 views
Hi everyone,
we applied the ST FWU reference solution on our own platform based on the STM32MP157F.
The solution was taken and adapted from the ST Yocto layer meta-st-ota (https://github.com/PRG-MPU-CUST/meta-st-ota).
Summary
When performing consecutive updates using the ST FWU reference implementation (TF-A FWU metadata + RAUC + post-install.sh + rauc-mark-good.service), the FWU rollback boot counter keeps decreasing across successful updates.
Expectation: after each successful boot of a newly updated bank (and rauc-mark-good.service finishing successfully), the FWU boot counter should be reset to the initial value (4 in this setup).
Actual: the FWU boot counter is decremented (4 → 3 → 2) with each update cycle, even though the system was marked good.
This suggests that the rollback counter is not being reset by the rauc-mark-good integration in the ST FWU reference solution.
(full log is attached, including metadata content printed in hexa after each step)
Reproduction and actual behavior
Boot fresh image (Bank A active).
Observe TFA logs: TF-A selects bank 0 (A).
INFO: Use primary FWU-Metadata
INFO: Try load metadata id=12...
NOTICE: Active index: 0, bank state: 252
NOTICE: Selecting to boot from bank 0Simulate first update in Linux (A → B)
On bank A:/usr/lib/rauc/post-install.shcurrent_boot_slot=A
...
active boot is B
boot count is enabledThen reboot:
rebootFirst boot after first update (Bank B active)
Observe TF-A logs:INFO: Use primary FWU-Metadata
INFO: Try load metadata id=12...
NOTICE: Active index: 1, bank state: 254NOTICE: Fwu bootcount 4 NOTICE:Selecting to boot from bank 1In Linux, rauc-mark-good runs and succeeds:
systemctl status rauc-mark-goodrauc-mark-good.service - Rauc Good-marking Service Main PID: 375 (code=exited, status=0/SUCCESS)
Dec 11 10:19:46 stm32mp15-pb2-base-mx sh[376]: rauc status: marked slot(s) rootfs.1 as good-> Expectation here: bootcount should now be reset back to 4 (for next update).
Simulate second consecutive update in Linux (B → A)
On bank B:/usr/lib/rauc/post-install.shcurrent_boot_slot=B...active boot is Aboot count is enabledThen reboot:
rebootSecond boot after second update (Bank A active)
TF-A logs now show that the bootcounter decreased:
INFO: Use primary FWU-MetadataINFO: Try load metadata id=12...NOTICE: Active index: 0, bank state: 254NOTICE: Fwu bootcount 3NOTICE: Selecting to boot from bank 0In Linux, again rauc-mark-good runs and reports success:
rauc-mark-good.service - Rauc Good-marking Service Main PID: 337 (code=exited, status=0/SUCCESS)Dec 11 10:25:50 stm32mp15-pb2-base-mx sh[342]: rauc status: marked slot(s) rootfs.0 as goodSimulate third update (A → B)
On bank A:
/usr/lib/rauc/post-install.shOutput:
current_boot_slot=A...active boot is B boot count is enabledThen reboot:
rebootThird boot after third update (Bank B active)
TF-A logs:
INFO: Use primary FWU-MetadataINFO: Try load metadata id=12...NOTICE: Active index: 1, bank state: 254NOTICE:Fwu bootcount 2NOTICE: Selecting to boot from bank 1
Expected behavior
After each successful boot of a newly updated bank and successful execution of rauc-mark-good.service, the FWU boot counter for that bank is reset to the initial value 4.
- And not 4 -> 3 -> 2