Skip to main content
Associate
Jun 28, 2024 8:00 AM UTC
Question

FreeRTOS systick

Originally posted in MCUs forum; moved to MPUs, as STM32MP is an MPU - not an MCU.


Hello Everyone,

I am working with FreeRTOS on an STM32MP157CAA and configuring the CM4 core in engineering mode using CubeIDE. According to the documentation, it's necessary to select a timer other than SysTick for the HAL timebase. However, in CubeIDE, under the SYS settings in the Pinout tab, I only see SysTick available as an option.

When I generate the code, I receive the following warning:

 

WARNING:
When RTOS is used, it is strongly recommended to use a HAL timebase source other than the SysTick. The HAL time base source can be changed from the Pinout tab under SYS.

 

Despite this, I am unable to select any other timebase source besides SysTick.

Could anyone provide guidance on how to configure a different HAL timebase source for FreeRTOS in this setup? Any advice or workaround would be greatly appreciated.

Thank you!

This topic has been closed for replies.

11 replies

AScha.3
Super User
Jun 28, 2024 8:36 AM UTC

Hi,

just give it (select in Cube...) a timer , you anyway not need for your program, i took TIM6 :

AScha3_0-1719563724346.png

Then it uses this and adjust it...you dont need to care about it.

If you feel a post has answered your question, please click on " Best Answer ".
YasirRAuthor
Associate
Jun 28, 2024 8:45 AM UTC

Hi AScha.3,

Thank you for your response. I understand what you mean. As I mentioned, I am unable to select any other timer; only SysTick is available as an option. Unlike in your case, I do not see any other timers like TIM6 highlighted for selection.

Do I need to configure anything else to enable the other timers, or is there another step I am missing to make these timers available for selection? Any guidance would be greatly appreciated.

 

Please have a look on the attached picture.

 

AScha.3
Super User
Jun 28, 2024 8:52 AM UTC

Hmmm...

1. you can only select timers, that are not used (by you), state : grey, unused on left side.

2. timers (in clock tree need a clock...) check in clock tree, you have clocks everywhere:

AScha3_0-1719564631630.png

 

If you feel a post has answered your question, please click on " Best Answer ".