Skip to main content
SMang.1
Associate II
Oct 15, 2020 4:31 PM UTC
Question

FreeRtos Debug issues on M4 core STM32MP1

Hi,

I am currently using the STM32MP1-DK1 board in engineering mode

When I am debugging the program and stepping instruction by instruction in IAR, the debugging process is lost at a time during the execution.

I can execute the program and and I can insert breakpoint wherever I want. But, before the instruction msr msp, r0 in the function vPortStartFirstTask in the file portasm.s has been executing, if we stop the program execution by inserting a breakpoint, the debugging process is lost with the error:

A vector table read fault has occurred.

The processor has escalated a configurable-priority exception to HardFault.   An MPU or Execute Never (XN) default memory map access violation has occurred on an instruction fetch (CFSR.IACCVIOL, MMFAR).   A precise data access error has occurred (CFSR.PRECISERR, BFAR) at data address 0x34020000. Exception occured at PC = 0x1000ced8, LR = 0x10006e9d

This topic has been closed for replies.

1 reply

AntonioST
ST Employee
Oct 15, 2020 4:42 PM UTC