Skip to main content
Mohand
Visitor II
May 20, 2024 9:26 AM UTC
Question

Firmware Deployment on STM32MP157D M4 Core

I am working on building a Yocto-based Linux distribution for the STM32MP157D SoC. I have already set up the process to build the Linux image successfully. However, I need guidance on the following:

Deploying Firmware on M4 Core

  • What is the correct procedure to deploy firmware on the M4 coprocessor core of the STM32MP157D?
  • Are there any best practices or considerations I should keep in mind while deploying firmware on the M4 core?

Communication between A7 and M4 Cores

  • How can I establish communication between the main A7 core (running Linux) and the M4 coprocessor core?
  • Are there any examples or sample code available to demonstrate the communication between the two cores?

I would greatly appreciate any guidance, documentation references, or code examples that could help me accomplish these tasks efficiently. Thank you in advance for your assistance.

This topic has been closed for replies.

1 reply

Associate II
Jul 2, 2024 6:10 AM UTC