Skip to main content
Visitor II
Mar 8, 2024 11:02 AM UTC
Question

Failing to build QT for stm32mp157f-dk2

Greetings!
I'm new to the stm32 community.

I am trying to build distribution package with qt following this guide https://wiki.st.com/stm32mpu/index.php/STM32MP1_Distribution_Package.

During the build with the command “bitbake -k st-example-image-qt” I encounter the following error

Full error logs attached

 

ERROR: All buildable tasks have been run but the build is incomplete (--continue mode). Errors for the tasks that failed will have been printed above.

ERROR: Command execution failed: 1

 

Summary: There were 2 WARNING messages shown.

Summary: There were 9 ERROR messages shown, returning a non-zero exit code.

 

When I try to build qtwebkit separately using the “bitbake qtwebkit” command I encounter the following error

Full error logs attached

| WARNING: exit code 1 from a shell command.

| ERROR: Function failed: do_compile (log file is located at /home/werent4/linux_source/Distribution-package/openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/x86_64-linux/m4-native/1.4.18-r0/temp/log.do_compile.509181)

ERROR: Task (/home/werent4/linux_source/Distribution-package/openstlinux-4.19-thud-mp1-19-02-20/layers/openembedded-core/meta/recipes-devtools/m4/m4-native_1.4.18.bb:do_compile) failed with exit code '1'

NOTE: Tasks Summary: Attempted 195 tasks of which 0 didn't need to be rerun and 1 failed.

NOTE: Writing buildhistory

 

Summary: 1 task failed:

  /home/werent4/linux_source/Distribution-package/openstlinux-4.19-thud-mp1-19-02-20/layers/openembedded-core/meta/recipes-devtools/m4/m4-native_1.4.18.bb:do_compile

Summary: There were 2 WARNING messages shown.

 

I'm using Ubuntu 22.04.4 LTS

free -m

               total        used        free      shared  buff/cache   available

Mem:           32073        1805         693          56       29574       29757

Swap:           9215           0        9215

 

I tried in the local.conf file

PARALLEL_MAKE = "-j 1"

BB_NUMBER_THREADS = "1"

I tried to patch it with this patch:
https://git.yoctoproject.org/poky/tree/meta/recipes-devtools/m4/m4/m4-1.4.18-glibc-change-work-around.patch?h=thud&id=95ca077ab871ceff46c2052f324f879a1d624ff4

 

Tried changing ROOTFS_PARTITION_SIZE to “1400000”

Solutions that I found on the Internet and tried
https://stackoverflow.com/questions/67500482/petalinux-project-build-failing-with-m4-native-1-4-18-r0-do-compile-failed-on-ho
https://community.st.com/t5/stm32-mpus-embedded-software/what-is-the-process-for-initializing-the-openembedded-build/m-p/407331
https://community.st.com/t5/stm32-mpus-embedded-software/getting-failure-while-compiling-qtwebkit-for-yocto/td-p/289256
https://medium.com/@BradenSunwold/how-to-set-up-stm32mp1-with-qt-part-1-7576eec8f1fe
https://medium.com/hi-z-labs/yocto-qt5-b2qt-build-fails-on-qtlocation-or-qtwebengine-with-cryptic-gcc-error-1051a7effe3a

https://medium.com/@BradenSunwold/how-to-set-up-stm32mp1-with-qt-part-1-7576eec8f1fe

Any suggestions are welcome!
Looking forward to hearing from you!

 

 

This topic has been closed for replies.

1 reply

Jean-Marc B
ST Employee
Mar 8, 2024 1:23 PM UTC

Hello @weren4 

From what I see from your logs, your image is really old as based on ecosystem 1.2! I would recommend to upgrade to the last ecosystem release 5.0.2

Best regards,

--JM