Question
Ethernet not working in u-boot: "Could not get PHY for ethernet@5800a000: addr 0 phy_connect() failed"
hi,
I am working with a custom board based on the STM32MP157C.
I use a lan9303 chip which is acting as a switch for ethernet. In the linux kernel, there are no problems with the ethernet but I can't get it to work in u-boot. Even when I use the same Device-Tree layout for the ethernet and phy.
The address 0 is the same thats used by the kernel but u-boot doesn't seem to find the phy there.
The device tree for ethernet looks like this:
ðernet0 {
status = "okay";
pinctrl-0 = <ðernet0_rmii_pins_a>;
pinctrl-1 = <ðernet0_rmii_pins_sleep_a>;
pinctrl-names = "default", "sleep";
phy-mode = "rmii";
};
&pinctrl {
ethernet0_rmii_pins_a: rmii-0 {
pins1 {
pinmux = <STM32_PINMUX('G', 13, AF11)>, /* ETH1_RMII_TXD0 */
<STM32_PINMUX('G', 14, AF11)>, /* ETH1_RMII_TXD1 */
<STM32_PINMUX('B', 11, AF11)>, /* ETH1_RMII_TX_EN */
<STM32_PINMUX('A', 1, AF11)>, /* ETH1_RMII_REF_CLK */
<STM32_PINMUX('A', 2, AF11)>, /* ETH1_MDIO */
<STM32_PINMUX('C', 1, AF11)>; /* ETH1_MDC */
bias-disable;
drive-push-pull;
slew-rate = <2>;
};
pins2 {
pinmux = <STM32_PINMUX('C', 4, AF11)>, /* ETH1_RMII_RXD0 */
<STM32_PINMUX('C', 5, AF11)>, /* ETH1_RMII_RXD1 */
<STM32_PINMUX('A', 7, AF11)>; /* ETH1_RMII_CRS_DV */
bias-disable;
};
};
ethernet0_rmii_pins_sleep_a: rmii-sleep-0 {
pins1 {
pinmux = <STM32_PINMUX('G', 13, ANALOG)>, /* ETH1_RMII_TXD0 */
<STM32_PINMUX('G', 14, ANALOG)>, /* ETH1_RMII_TXD1 */
<STM32_PINMUX('B', 11, ANALOG)>, /* ETH1_RMII_TX_EN */
<STM32_PINMUX('A', 2, ANALOG)>, /* ETH1_MDIO */
<STM32_PINMUX('C', 1, ANALOG)>, /* ETH1_MDC */
<STM32_PINMUX('C', 4, ANALOG)>, /* ETH1_RMII_RXD0 */
<STM32_PINMUX('C', 5, ANALOG)>, /* ETH1_RMII_RXD1 */
<STM32_PINMUX('A', 1, ANALOG)>, /* ETH1_RMII_REF_CLK */
<STM32_PINMUX('A', 7, ANALOG)>; /* ETH1_RMII_CRS_DV */
};
};
};For the phy like this:
&mdio0 {
phy0: ethernet-phy@0 {
compatible = "ethernet-phy-id0022.1622";
reg = <0>;
};
};This is basically the same as the device tree configuration for the Kernel, but its not working.
Maybe someone here can help me.