Skip to main content
SigmaPrime
Associate III
Oct 26, 2020 10:18 PM UTC
Question

Ethernet does not work

Hello everybody,

Here is my problem. I am using the buildroot distro instead of OpenSTLinux and want to

connect my STM32 via ethernet using SSH. I use MobaXterm as remote control software.

P.s After a system boot I get the following response although the ethernet LEDs are not blinking

buildroot login: [ 4.237860] stm32-dwmac 5800a000.ethernet eth0: Link 
is Up - 1Gbps/Full - flow control rx/tx
[ 4.251707] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

After ifconfig -a I get the following response:

eth0 Link encap:Ethernet HWaddr 00:80:E1:42:6B:16
 
 inet addr:192.168.8.45 Bcast:192.168.8.255 
 
Mask:255.255.255.0
 
 inet6 addr: fe80::280:e1ff:fe42:6b16/64 Scope:Link
 
 UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
 
 RX packets:107 errors:0 dropped:0 overruns:0 frame:0
 
 TX packets:11 errors:0 dropped:0 overruns:0 carrier:0
 
 collisions:0 txqueuelen:1000
 
 RX bytes:10299 (10.0 KiB) TX bytes:866 (866.0 B)
 
 Interrupt:60 Base address:0x8000

This configuration was generated manually by etc / network and then nano

Interfaces where it says:

auto lo
iface lo inet loopback
# Configure eth0 with static IP
auto eth0
iface eth0 inet static
 address 192.168.8.45
 network 192.168.8.0
 netmask 255.255.255.0
 broadcast 192.168.8.255
 gateway 192.168.8.1
 dns-nameservers 192.168.8.1
 
 
# Configure eth0 with dhcp IP
# auto eth0
# iface eth0 inet dhcp

My setup is made like this. My PC is connected to WiFi through one Huawei Giga Cube and the STM32 are connected to my PC by a Ethernet cable.

If I go into Windows cmd and use ipconfig / all then I get the following output:

Windows IP Configuration
 
 Host Name . . . . . . . . . . . . : ...
 Primary Dns Suffix . . . . . . . :
 Node Type . . . . . . . . . . . . : Broadcast
 IP Routing Enabled. . . . . . . . : No
 WINS Proxy Enabled. . . . . . . . : No
 
Ethernet adapter Ethernet:
 
 Media State . . . . . . . . . . . : Media disconnected
 Connection-specific DNS Suffix . :
 Description . . . . . . . . . . . : Intel(R) Ethernet Connection (6) 
I219-V
 Physical Address. . . . . . . . . : 48-2A-E3-50-1B-76
 DHCP Enabled. . . . . . . . . . . : Yes
 Autoconfiguration Enabled . . . . : Yes
 
Unknown adapter NordLynx:
 
 Connection-specific DNS Suffix . :
 Description . . . . . . . . . . . : NordLynx Tunnel
 Physical Address. . . . . . . . . :
 DHCP Enabled. . . . . . . . . . . : No
 Autoconfiguration Enabled . . . . : Yes
 Link-local IPv6 Address . . . . . : 
fe80::8df6:2969:45f4:3946%14(Preferred)
 Autoconfiguration IPv4 Address. . : 169.254.57.70(Preferred)
 Subnet Mask . . . . . . . . . . . : 255.255.0.0
 Default Gateway . . . . . . . . . :
 DNS Servers . . . . . . . . . . . : fec0:0:0:ffff::1%1
 fec0:0:0:ffff::2%1
 fec0:0:0:ffff::3%1
 NetBIOS over Tcpip. . . . . . . . : Enabled
 
Ethernet adapter Ethernet 2:
 
 Connection-specific DNS Suffix . :
 Description . . . . . . . . . . . : Realtek USB GbE Family Controller
 Physical Address. . . . . . . . . : 00-E0-4C-68-2E-FD
 DHCP Enabled. . . . . . . . . . . : Yes
 Autoconfiguration Enabled . . . . : Yes
 Link-local IPv6 Address . . . . . : 
fe80::ddff:5546:f233:2654%19(Preferred)
 Autoconfiguration IPv4 Address. . : 169.254.38.84(Preferred)
 Subnet Mask . . . . . . . . . . . : 255.255.0.0
 Default Gateway . . . . . . . . . :
 DHCPv6 IAID . . . . . . . . . . . : 419487820
 DHCPv6 Client DUID. . . . . . . . : 
00-01-00-01-24-C3-57-40-48-2A-E3-50-1B-76
 DNS Servers . . . . . . . . . . . : fec0:0:0:ffff::1%1
 fec0:0:0:ffff::2%1
 fec0:0:0:ffff::3%1
 NetBIOS over Tcpip. . . . . . . . : Enabled
 
Ethernet adapter Ethernet 4:
 
 Media State . . . . . . . . . . . : Media disconnected
 Connection-specific DNS Suffix . :
 Description . . . . . . . . . . . : TAP-NordVPN Windows Adapter V9
 Physical Address. . . . . . . . . : 00-FF-E3-A4-9C-52
 DHCP Enabled. . . . . . . . . . . : Yes
 Autoconfiguration Enabled . . . . : Yes
 
Ethernet adapter Ethernet 5:
 
 Connection-specific DNS Suffix . :
 Description . . . . . . . . . . . : VirtualBox Host-Only Ethernet 
Adapter
 Physical Address. . . . . . . . . : 0A-00-27-00-00-1A
 DHCP Enabled. . . . . . . . . . . : No
 Autoconfiguration Enabled . . . . : Yes
 Link-local IPv6 Address . . . . . : 
fe80::b4ff:a90a:c8d:424a%26(Preferred)
 IPv4 Address. . . . . . . . . . . : 192.168.206.1(Preferred)
 Subnet Mask . . . . . . . . . . . : 255.255.255.0
 Default Gateway . . . . . . . . . :
 DHCPv6 IAID . . . . . . . . . . . : 1024065575
 DHCPv6 Client DUID. . . . . . . . : 
00-01-00-01-24-C3-57-40-48-2A-E3-50-1B-76
 DNS Servers . . . . . . . . . . . : fec0:0:0:ffff::1%1
 fec0:0:0:ffff::2%1
 fec0:0:0:ffff::3%1
 NetBIOS over Tcpip. . . . . . . . : Enabled
 
Unknown adapter LAN-Verbindung:
 
 Media State . . . . . . . . . . . : Media disconnected
 Connection-specific DNS Suffix . :
 Description . . . . . . . . . . . : TAP-Windows Adapter V9
 Physical Address. . . . . . . . . : 00-FF-6A-9C-8E-76
 DHCP Enabled. . . . . . . . . . . : Yes
 Autoconfiguration Enabled . . . . : Yes
 
Wireless LAN adapter LAN-Verbindung* 1:
 
 Media State . . . . . . . . . . . : Media disconnected
 Connection-specific DNS Suffix . :
 Description . . . . . . . . . . . : Microsoft Wi-Fi Direct Virtual 
Adapter #3
 Physical Address. . . . . . . . . : 24-EE-9A-7C-90-D0
 DHCP Enabled. . . . . . . . . . . : Yes
 Autoconfiguration Enabled . . . . : Yes
 
Wireless LAN adapter LAN-Verbindung* 12:
 
 Media State . . . . . . . . . . . : Media disconnected
 Connection-specific DNS Suffix . :
 Description . . . . . . . . . . . : Microsoft Wi-Fi Direct Virtual 
Adapter #4
 Physical Address. . . . . . . . . : 26-EE-9A-7C-90-CF
 DHCP Enabled. . . . . . . . . . . : Yes
 Autoconfiguration Enabled . . . . : Yes
 
Wireless LAN adapter WLAN:
 
 Connection-specific DNS Suffix . :
 Description . . . . . . . . . . . : Intel(R) Wireless-AC 9560 160MHz
 Physical Address. . . . . . . . . : 24-EE-9A-7C-90-CF
 DHCP Enabled. . . . . . . . . . . : Yes
 Autoconfiguration Enabled . . . . : Yes
 Link-local IPv6 Address . . . . . : 
fe80::ac7a:f511:a7ab:a012%23(Preferred)
 IPv4 Address. . . . . . . . . . . : 192.168.8.124(Preferred)
 Subnet Mask . . . . . . . . . . . : 255.255.255.0
 Lease Obtained. . . . . . . . . . : Monday, October 26, 2020 9:45:02 
PM
 Lease Expires . . . . . . . . . . : Tuesday, October 27, 2020 
10:28:23 PM
 Default Gateway . . . . . . . . . : 192.168.8.1
 DHCP Server . . . . . . . . . . . : 192.168.8.1
 DHCPv6 IAID . . . . . . . . . . . : 287633050
 DHCPv6 Client DUID. . . . . . . . : 
00-01-00-01-24-C3-57-40-48-2A-E3-50-1B-76
 DNS Servers . . . . . . . . . . . : fe80::5625:eaff:fe6f:3ce6%23
 192.168.8.1
 NetBIOS over Tcpip. . . . . . . . : Enabled
 
Ethernet adapter Bluetooth-Netzwerkverbindung:
 
 Media State . . . . . . . . . . . : Media disconnected
 Connection-specific DNS Suffix . :
 Description . . . . . . . . . . . : Bluetooth Device (Personal Area 
Network)
 Physical Address. . . . . . . . . : 24-EE-9A-7C-90-D3
 DHCP Enabled. . . . . . . . . . . : Yes
 Autoconfiguration Enabled . . . . : Yes
 
Ethernet adapter vEthernet (Default Switch):
 
 Connection-specific DNS Suffix . :
 Description . . . . . . . . . . . : Hyper-V Virtual Ethernet Adapter
 Physical Address. . . . . . . . . : 00-15-5D-65-E6-15
 DHCP Enabled. . . . . . . . . . . : No
 Autoconfiguration Enabled . . . . : Yes
 Link-local IPv6 Address . . . . . : 
fe80::74c4:a88f:e305:e735%22(Preferred)
 IPv4 Address. . . . . . . . . . . : 192.168.238.241(Preferred)
 Subnet Mask . . . . . . . . . . . : 255.255.255.240
 Default Gateway . . . . . . . . . :
 DHCPv6 IAID . . . . . . . . . . . : 369104221
 DHCPv6 Client DUID. . . . . . . . : 
00-01-00-01-24-C3-57-40-48-2A-E3-50-1B-76
 DNS Servers . . . . . . . . . . . : fec0:0:0:ffff::1%1
 fec0:0:0:ffff::2%1
 fec0:0:0:ffff::3%1
 NetBIOS over Tcpip. . . . . . . . : Enabled
 
Ethernet adapter vEthernet (WSL):
 
 Connection-specific DNS Suffix . :
 Description . . . . . . . . . . . : Hyper-V Virtual Ethernet Adapter 
#2
 Physical Address. . . . . . . . . : 00-15-5D-3A-2A-A7
 DHCP Enabled. . . . . . . . . . . : No
 Autoconfiguration Enabled . . . . : Yes
 Link-local IPv6 Address . . . . . : 
fe80::2165:e63f:cd0d:3e86%80(Preferred)
 IPv4 Address. . . . . . . . . . . : 172.18.18.17(Preferred)
 Subnet Mask . . . . . . . . . . . : 255.255.255.240
 Default Gateway . . . . . . . . . :
 DHCPv6 IAID . . . . . . . . . . . : 1342182749
 DHCPv6 Client DUID. . . . . . . . : 
00-01-00-01-24-C3-57-40-48-2A-E3-50-1B-76
 DNS Servers . . . . . . . . . . . : fec0:0:0:ffff::1%1
 fec0:0:0:ffff::2%1
 fec0:0:0:ffff::3%1
 NetBIOS over Tcpip. . . . . . . . : Enabled

I hope that you can help me. Thank you all

This topic has been closed for replies.

4 replies

Olivier GALLIEN
ST Technical Moderator
Nov 5, 2020 3:17 PM UTC

Hi @SigmaPrime​ ,

Be aware that ST is not supporting buildroot solution directly, but only through some partner ( eg Bootlin) .

I suggest to have a look in our wiki , in case an article may guide you in the right direction, else try to get help from partner community.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SigmaPrime
Associate III
Nov 5, 2020 3:27 PM UTC

Thank you for your response.

I would say that they are not serious when responding to people. I managed to resolve the solution alone after multiple tries.

It appeared that my system configuration wasn't correct and that some packages were missing. I had to contact Rasp community to get the right info.

Buildroot forum is messy and when I want to upload multiple files with a modest size I can't do that so explaining my situation is really difficult when turning to them.

Fee
Associate II
Nov 6, 2020 6:18 AM UTC

Hi,

for people wanting to start using buildroot for the STM32MP1 there is a GitHub Repo with a buildroot example for the STM32MP1. I'm pretty sure it doesn't contain a ssh packet at the start but you can easily use this as a starting point and activate something like dropbear. Helped me at the start using buildroot a lot besides some Bootlin blog articles.

Github repo:

https://github.com/schenkmi/buildroot-op-tee-stm32mp1

Cheers

SigmaPrime
Associate III
Nov 6, 2020 9:45 AM UTC

Thank you gonna check it out