Skip to main content
SigmaPrime
Associate III
Dec 10, 2020 3:48 PM UTC
Question

Error: Task do_populate_sdk in .... rdepends upon non-existent task do_package_write_deb

Hello

I am trying to build an Image based on the Yocto Project for my stm32mp157c-DK2 according to st-wiki.

When I try to build the image I get the following error.

ERROR: Task do_populate_sdk in /home/mehdi/Distribution-Package/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb rdepends upon non-existent task do_package_write_deb in /home/mehdi/Distribution-Package/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb ERROR: Command execution failed: 1

What did I miss or what did I do wrong in my local.conf file ?

Best regards.

I can share with you the content of the file.

This topic has been closed for replies.

3 replies

Olivier GALLIEN
ST Technical Moderator
Dec 14, 2020 2:23 PM UTC

Hi @SigmaPrime​ ,

st-wiki page you mention didn't cover any kind of customization but just building delivered image.

What are you trying to achieve ?

Where does this local.conf come from ?

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SigmaPrime
Associate III
Dec 14, 2020 3:06 PM UTC

Thank you for your response Oliver.

I know. The wiki page is simply a basic support on how to build an image for my stm32.

I simply wanted to add some packages to be integrated into the build.

I don't understand why some packages are not able to be built properly although their recipes are in the layers provided by the wiki.

I simply want to learn how to configure my image based on the layers provided:

-Adding packages to be used

-Configuring the Linux Tree through menuconfig

I used to work with other distros like buildroot and the procedure to do these to steps was way less complicated than using Yocto (or a Yocto based project).

I am still learning that's why it is blurry in my mind.

The local.conf is located at ~/DP1/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1-disco/conf.

I simply used the IMAGE_INSTALL_append to add packages. It appears that this will not work with all packages.

Thank you.