Skip to main content
AMill.9
Associate
Mar 15, 2023 6:38 AM UTC
Solved

Error activating SPI5 using Buildroot external configuration

I'm using the STM32MP157F-DK2-ND evaluation board and getting an error when I try to enable SPI5.

I have researched previous posts with this error

https://community.st.com/s/question/0D53W000006FjAUSA0/error-activating-spi-module-in-yocto-linux-project

https://community.st.com/s/question/0D53W00000GZlRVSA1/enabling-devspidevxx-on-openstlinux

https://community.st.com/s/question/0D53W00000RS3ynSAD/how-can-i-enable-spi5-on-stm32mp157dk1

And reviewed relevant documentation

https://wiki.st.com/stm32mpu/wiki/How_to_use_SPI_from_Linux_userland_with_spidev

https://wiki.st.com/stm32mpu/wiki/SPI_overview

https://wiki.st.com/stm32mpu/wiki/SPI_device_tree_configuration

I've also ensured these options are checked in make linux-menuconfig

https://wiki.st.com/stm32mpu/wiki/SPI_overview#Kernel_configuration

Still, I cannot figure out why the clock isn't running.

[ 1.533147] spi_stm32 44009000.spi: clk rate = 0               

[ 1.536942] spi_stm32: probe of 44009000.spi failed with error -22  

 I 'm using the buildroot config: st_stm32mp157f_dk2_demo_defconfig provided by github buildroot-external-st repository (new member so can't add link)

After generating from CubeMX I added the following user code in my linux-dts and uboot-dts files:

&spi5{

pinctrl-names = "default", "sleep";

pinctrl-0 = <&spi5_pins_mx>;

pinctrl-1 = <&spi5_sleep_pins_mx>;

 cs-gpios= <&gpiof 6 0>;

status = "okay";

 

/* USER CODE BEGIN spi5 */

 spidev@0{

  compatible = "linux,spidev";

  reg = <0>;

  spi-max-frequency = <4000000>;

 };

/* USER CODE END spi5 */

};

I also ensured:

CLK_SPI2S23_PLL3Q

CLK_SPI45_PCLK2

are set in my tfa-dts file

I ensured these settings are getting built correctly by downloading the output from:

output/build/linux-custom/

I would appreciate help to troubleshoot this and any debug tools I can use to figure out this issue. Thanks!

This topic has been closed for replies.
Kevin HUBER
Kevin HUBERBest answer
ST Employee
Mar 29, 2023 1:40 PM UTC

Hello @AMill.9​ ,

I can see that you are using:

+	compatible = "linux,spidev";

In the spidev.c it is indicated:

	/*
	 * spidev should never be referenced in DT without a specific
 	 * compatible string, it is a Linux implementation thing
 	 * rather than a description of the hardware.
 	 */
 	WARN(spi->dev.of_node &&
 	 of_device_is_compatible(spi->dev.of_node, "spidev"),
 	 "%pOF: buggy DT: spidev listed directly in DT\n", spi->dev.of_node);

And below you have the list of compatible field possible in a DT:

static const struct of_device_id spidev_dt_ids[] = {
	{ .compatible = "rohm,dh2228fv" },
	{ .compatible = "lineartechnology,ltc2488" },
	{ .compatible = "semtech,sx1301" },
	{ .compatible = "lwn,bk4" },
	{ .compatible = "dh,dhcom-board" },
	{ .compatible = "menlo,m53cpld" },
	{ .compatible = "cisco,spi-petra" },
	{ .compatible = "micron,spi-authenta" },
	{},

You must use one of these compatible fields in your DTS to have spidev functional.

And be sure to have enabled these linux configurations described in the wiki: https://wiki.st.com/stm32mpu/wiki/SPI_overview#Kernel_configuration

Hope it helps,

Best regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

3 replies

AMill.9
AMill.9Author
Associate
Mar 15, 2023 8:11 PM UTC

Should I try to do a minimal build with only SPI5 enabled instead of all this other crap?

AMill.9
AMill.9Author
Associate
Mar 16, 2023 10:35 PM UTC

PLEASE can I get some help? I will even pay. I need to get this working asap as it's holding up the project.

Kevin HUBER
Kevin HUBERBest answer
ST Employee
Mar 29, 2023 1:40 PM UTC

Hello @AMill.9​ ,

I can see that you are using:

+	compatible = "linux,spidev";

In the spidev.c it is indicated:

	/*
	 * spidev should never be referenced in DT without a specific
 	 * compatible string, it is a Linux implementation thing
 	 * rather than a description of the hardware.
 	 */
 	WARN(spi->dev.of_node &&
 	 of_device_is_compatible(spi->dev.of_node, "spidev"),
 	 "%pOF: buggy DT: spidev listed directly in DT\n", spi->dev.of_node);

And below you have the list of compatible field possible in a DT:

static const struct of_device_id spidev_dt_ids[] = {
	{ .compatible = "rohm,dh2228fv" },
	{ .compatible = "lineartechnology,ltc2488" },
	{ .compatible = "semtech,sx1301" },
	{ .compatible = "lwn,bk4" },
	{ .compatible = "dh,dhcom-board" },
	{ .compatible = "menlo,m53cpld" },
	{ .compatible = "cisco,spi-petra" },
	{ .compatible = "micron,spi-authenta" },
	{},

You must use one of these compatible fields in your DTS to have spidev functional.

And be sure to have enabled these linux configurations described in the wiki: https://wiki.st.com/stm32mpu/wiki/SPI_overview#Kernel_configuration

Hope it helps,

Best regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.