Question
Enabling USART6 as a serial Port
Hello ST,
We are trying to enable USART6 as a serial console, in the stm32mp257f-dk board, we have builded the SDK using Openstlinux "Distribution package", I had done the below changes in the stm32mp257f-dk.dts device tree present in the kernel-source and u-boot directory :
aliases {
serial1 = &usart6;
};
chosen {
stdout-path = "serial1:115200n8";
#address-cells = <2>;
#size-cells = <2>;
ranges;
};
&usart2 {
pinctrl-names = "default", "idle", "sleep";
pinctrl-0 = <&usart2_pins_a>;
pinctrl-1 = <&usart2_idle_pins_a>;
pinctrl-2 = <&usart2_sleep_pins_a>;
/delete-property/dmas;
/delete-property/dma-names;
status = "okay";
};
&usart6 {
pinctrl-names = "default", "idle", "sleep";
pinctrl-0 = <&usart6_pins_a>;
pinctrl-1 = <&usart6_idle_pins_a>;
pinctrl-2 = <&usart6_sleep_pins_a>;
uart-has-rtscts;
status = "okay";
};And also modified the stm32mp257f-dk-u-boot.dtsi device tree and pin configurations as shown below :
&usart6 {
bootph-all;
};
&usart6_pins_a {
bootph-all;
pins1 {
bootph-all;
};
pins2 {
bootph-all;
};
};But getting the below error :
E/TC:0 stm32_serc_handle_ilac:133 SERC exceptions [63:32]: 0x10
E/TC:0 stm32_serc_handle_ilac:139 SERC exception ID: 36root@stm32mp25-disco-e3-cc-91:~# stty -F /dev/ttySTM1
E/TC:0 stm32_serc_handle_ilac:133 SERC exceptions [63:32]: 0x10
E/TC:0 stm32_serc_handle_ilac:139 SERC exception ID: 36
[ 426.789010] SError Interrupt on CPU0, code 0x00000000bf000002 -- SError
[ 426.789029] CPU: 0 PID: 1625 Comm: stty Tainted: G O 6.6.78 #1
[ 426.789039] Hardware name: STMicroelectronics STM32MP257F-DK Discovery Board (DT)
[ 426.789044] pstate: 80000005 (Nzcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 426.789053] pc : stm32_usart_rx_dma_start_or_resume+0x80/0x234
[ 426.789072] lr : stm32_usart_startup+0x8c/0x130
[ 426.789082] sp : ffff8000839db950
[ 426.789085] x29: ffff8000839db950 x28: ffff00008c143e40 x27: 0000000000020800
[ 426.789101] x26: ffff800081037828 x25: ffff800081037468 x24: 0000000000000000
[ 426.789113] x23: 0000000000000000 x22: ffff000081b23800 x21: ffff8000819ed048
[ 426.789126] x20: 0000000000000000 x19: ffff800081b08210 x18: ffffffffffffffff
[ 426.789138] x17: 0000000000000000 x16: 0000000000000000 x15: ffff8000839db700
[ 426.789149] x14: 0000000000000001 x13: 006c61697265732e x12: 0000000000000000
[ 426.789161] x11: ffff0000890e2920 x10: ffffffffffffffc0 x9 : ffffffffffffffff
[ 426.789174] x8 : 0000000000000228 x7 : 0000000000000000 x6 : 0000000000000000
[ 426.789185] x5 : ffff000081bad748 x4 : ffff000081bad808 x3 : 0000000000000000
[ 426.789197] x2 : ffff800081dd5000 x1 : 0000000000000000 x0 : ffff0000824f2080
[ 426.789211] Kernel panic - not syncing: Asynchronous SError Interrupt
[ 426.789216] CPU: 0 PID: 1625 Comm: stty Tainted: G O 6.6.78 #1
[ 426.789223] Hardware name: STMicroelectronics STM32MP257F-DK Discovery Board (DT)
[ 426.789227] Call trace:
[ 426.789231] dump_backtrace+0x94/0x114
[ 426.789245] show_stack+0x18/0x24
[ 426.789256] dump_stack_lvl+0x48/0x60
[ 426.789265] dump_stack+0x18/0x24
[ 426.789272] panic+0x324/0x380
[ 426.789282] nmi_panic+0x8c/0x90
[ 426.789290] arm64_serror_panic+0x6c/0x78
[ 426.789298] do_serror+0x3c/0x70
[ 426.789304] el1h_64_error_handler+0x30/0x48
[ 426.789314] el1h_64_error+0x64/0x68
[ 426.789321] stm32_usart_rx_dma_start_or_resume+0x80/0x234
[ 426.789331] stm32_usart_startup+0x8c/0x130
[ 426.789341] uart_startup+0x13c/0x2fc
[ 426.789351] uart_port_activate+0x34/0x9c
[ 426.789360] tty_port_open+0x8c/0x13c
[ 426.789371] uart_open+0x1c/0x30
[ 426.789380] tty_open+0x138/0x6dc
[ 426.789388] chrdev_open+0xbc/0x208
[ 426.789400] do_dentry_open+0x1b0/0x524
[ 426.789413] vfs_open+0x2c/0x38
[ 426.789420] path_openat+0xb14/0xdf0
[ 426.789430] do_filp_open+0x9c/0x14c
[ 426.789440] do_sys_openat2+0xc4/0x104
[ 426.789447] __arm64_sys_openat+0x64/0xac
[ 426.789455] invoke_syscall+0x48/0x114
[ 426.789466] el0_svc_common.constprop.0+0x40/0xe0
[ 426.789476] do_el0_svc+0x1c/0x28
[ 426.789486] el0_svc+0x38/0xc8
[ 426.789493] el0t_64_sync_handler+0x120/0x12c
[ 426.789501] el0t_64_sync+0x190/0x194
[ 426.789510] SMP: stopping secondary CPUs
[ 426.789527] Kernel Offset: disabled
[ 426.789529] CPU features: 0x0,00000000,00020000,0000421b
[ 426.789536] Memory Limit: none
[ 427.047254] ---[ end Kernel panic - not syncing: Asynchronous SError Interrupt ]---
E/TC:1 Panic 'Watchdog' at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r2/core/drivers/stm32_iwdg.c:218 <stm32_iwdg_it_handler>then the device gets rebooted.
Can you suggest a simple straight forward documentation for resolving the SREC error as I am new the technology :)