Skip to main content
Lead
Mar 3, 2026 7:33 AM UTC
Solved

Driver stm32_tamp_nvram on node nvram@46010100 failed

I having some issues with nvram in op-tee.

I don't know what this happen. It seems that op-tee want to say to me that 0xffff0006 is TEE_ERROR_BAD_PARAMETERS. In this case, I don't use any tamper and don't have LSE.

I think this is a bug because my ST TF-A and ST Op-tee assumes that LSE must be available to proceed. I made a specific hack in ST TF-A that avoids the LSE configuration to continue working. When ST TF-A was starting. It was going to enable clock ID 5, which is LSE, no matter if I have LSE disabled or enable. An if-statement solved this issue.

Do you have any clue what's can be the cause of this?

Processor: STM32MP257FAK

 

F/TC:0 0 process_probe_list:657 Probe loop 6 after 4 for deferral(s)
D/TC:0 0 print_probe_list:504 Probe list: 3 elements
D/TC:0 0 print_probe_list:506 |- Driver stm32-gpu probes on node gpu@48280000
D/TC:0 0 print_probe_list:506 |- Driver stm32-tamp probes on node tamp@46010000
D/TC:0 0 print_probe_list:506 |- Driver stm32-cpu probes on node cpu@0
D/TC:0 0 print_probe_list:510 `- Probe list end
D/TC:0 0 print_probe_list:516 Failed list: 0 elements
D/TC:0 0 print_probe_list:521 `- Failed list end
F/TC:0 0 probe_driver_node:543 Probing stm32-cpu on node cpu@0
D/TC:0 0 probe_driver_node:556 element: stm32-cpu on node cpu@0 deferred 1 time(s)
F/TC:0 0 probe_driver_node:543 Probing stm32-tamp on node tamp@46010000
D/TC:0 0 gic_it_set_cpu_mask:410 cpu_mask: writing 0x3ff0000 to 0x72a1082c
D/TC:0 0 gic_it_set_cpu_mask:412 cpu_mask: 0x3030000
D/TC:0 0 gic_it_set_prio:426 prio: writing 0x1 to 0x72a1042e
D/TC:0 0 stm32_tamp_parse_passive_conf:1649 Passive conf from dt: precharge=0, nb_sample=0, clk_div=32768
D/TC:0 0 stm32_tamp_parse_active_conf:1874 Active conf from dt: no filter clk_div=1
F/TC:0 0 stm32_tamp_probe:2057 STM32 TAMPER V3.4
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:636 Backup registers mapping :
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:637 ********START of zone 1********
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:638 Protection Zone 1-RIF1 begins at register: 0
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:639 Protection Zone 1-RIF2 begins at register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:641 Protection Zone 1-RIF2 ends at register: 127
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:643 ********END of zone 1********
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:644 ********START of zone 2********
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:645 Protection Zone 2-RIF1 begins at register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:647 Protection Zone 2-RIF2 begins at register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:649 Protection Zone 2-RIF2 ends at register: 0
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:652 ********END of zone 2********
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:653 ********START of zone 3********
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:654 Protection Zone 3-RIF1 begins at register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:656 Protection Zone 3-RIF0 begins at register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:658 Protection Zone 3-RIF2 begins at register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:660 Protection Zone 3-RIF2 ends at the last register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:661 ********END of zone 3********
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP1 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP2 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP3 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP4 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP5 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP6 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP7 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP8 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP9 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP10 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP11 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP12 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP14 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP15 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP1 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP2 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP3 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP4 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP5 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP6 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP7 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP8 disabled
F/TC:0 0 stm32_tamp_set_config:1163 Set passive conf 00000080
F/TC:0 0 stm32_tamp_set_config:1168 Set active conf1 00000000
F/TC:0 0 stm32_tamp_set_config:1172 Set active conf2 00000000
D/TC:0 0 add_node_to_probe:748 element: stm32_tamp_nvram on node nvram@46010100
D/TC:0 0 print_probe_list:504 Probe list: 3 elements
D/TC:0 0 print_probe_list:506 |- Driver stm32-gpu probes on node gpu@48280000
D/TC:0 0 print_probe_list:506 |- Driver stm32-cpu probes on node cpu@0
D/TC:0 0 print_probe_list:506 |- Driver stm32_tamp_nvram probes on node nvram@46010100
D/TC:0 0 print_probe_list:510 `- Probe list end
D/TC:0 0 print_probe_list:516 Failed list: 0 elements
D/TC:0 0 print_probe_list:521 `- Failed list end
D/TC:0 0 probe_driver_node:550 element: stm32-tamp on node tamp@46010000 initialized
F/TC:0 0 probe_driver_node:543 Probing stm32-gpu on node gpu@48280000
D/TC:0 0 probe_driver_node:556 element: stm32-gpu on node gpu@48280000 deferred 4 time(s)
F/TC:0 0 process_probe_list:657 Probe loop 7 after 5 for deferral(s)
D/TC:0 0 print_probe_list:504 Probe list: 3 elements
D/TC:0 0 print_probe_list:506 |- Driver stm32-cpu probes on node cpu@0
D/TC:0 0 print_probe_list:506 |- Driver stm32_tamp_nvram probes on node nvram@46010100
D/TC:0 0 print_probe_list:506 |- Driver stm32-gpu probes on node gpu@48280000
D/TC:0 0 print_probe_list:510 `- Probe list end
D/TC:0 0 print_probe_list:516 Failed list: 0 elements
D/TC:0 0 print_probe_list:521 `- Failed list end
F/TC:0 0 probe_driver_node:543 Probing stm32-gpu on node gpu@48280000
D/TC:0 0 probe_driver_node:556 element: stm32-gpu on node gpu@48280000 deferred 5 time(s)
F/TC:0 0 probe_driver_node:543 Probing stm32_tamp_nvram on node nvram@46010100
E/TC:0 0 probe_driver_node:565 Failed to probe stm32_tamp_nvram on node nvram@46010100: 0xffff0006
F/TC:0 0 probe_driver_node:543 Probing stm32-cpu on node cpu@0
D/TC:0 0 probe_driver_node:556 element: stm32-cpu on node cpu@0 deferred 2 time(s)
D/TC:0 0 process_probe_list:697 Unresolved dependencies after 7 rounds, 6 deferred
E/TC:0 0 probe_dt_drivers:902 Probe sequence result: 0x80000000
D/TC:0 0 print_probe_list:504 Probe list: 2 elements
D/TC:0 0 print_probe_list:506 |- Driver stm32-gpu probes on node gpu@48280000
D/TC:0 0 print_probe_list:506 |- Driver stm32-cpu probes on node cpu@0
D/TC:0 0 print_probe_list:510 `- Probe list end
D/TC:0 0 print_probe_list:516 Failed list: 1 elements
E/TC:0 0 print_probe_list:518 |- Driver stm32_tamp_nvram on node nvram@46010100 failed
D/TC:0 0 print_probe_list:521 `- Failed list end
E/TC:0 0 Panic at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r2/core/kernel/dt_driver.c:904 <probe_dt_drivers>
E/TC:0 0 TEE load address @ 0x82000000
E/TC:0 0 Call stack:
E/TC:0 0 0x82008140
E/TC:0 0 0x82046c74
E/TC:0 0 0x82042ca0
E/TC:0 0 0x82048980
E/TC:0 0 0x82007bac
E/TC:0 0 0x82007f44

 

DMårtBest answer
Lead
Mar 4, 2026 9:03 PM UTC

Hi @PatrickF 

I solved this by setting this inside &tamp of op-tee DT. The CubeMX assumes that &tamp is default OK and requires LSE as usual. I think it's not good to construct ST Op-tee and ST TF-A to just suit DK/EV.

&tamp {
 status = "disable";
};

 

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer

4 replies

PatrickF
ST Employee
Mar 3, 2026 4:15 PM UTC

HI @DMårt 

The fail sound linked to op-TEE init of TAMP Backup_registers (or at least init some security inside).

https://wiki.st.com/stm32mpu/wiki/STM32MP2_backup_registers


I'm not sure about that, but maybe this fail because the RTC/TAMP IP does not receive its ck_ker_rtc clock (default from LSE on our platforms, but could come from LSI or HSE/RTCDIV). or RTC/TAMP IP is not enabled (RTCEN).

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
DMårtAuthor
Lead
Mar 3, 2026 5:17 PM UTC

Hi @PatrickF 

In this case, my custom board does not have LSE. I assume that the TF-A and op-TEE is built to fit DK/EV.

I will look up the clocks and see why.

Do you have any registers I should look on at, more than RTCEN?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
PatrickF
ST Employee
Mar 4, 2026 8:54 AM UTC

Hi,
RTC/TAMP kernel clock source is defined by RTCSRC[1:0] in RCC_BDCR.

Notice that this field is write once and the register is write-protected by DBD3P in PWR_BDCR1.

Regards.

 

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent