Skip to main content
Associate II
Dec 3, 2025 4:54 AM UTC
Question

DP83867IRRGZT Ethernet DT configuration in stm32mp257f-ev1

 

The below device tree is for RTL8211F-CG, but i needed help with configuring DT for DP83867IRRGZT, which DT binding should i refer, and if possibly have a DT configured for DP83867IRRGZT, do share it.

 

Hoping for a quick reply,

Thanks in advance.

&eth1 {
	status = "disabled";
	pinctrl-0 = <&eth1_rgmii_pins_a &eth1_mdio_pins_a>;
	pinctrl-1 = <&eth1_rgmii_sleep_pins_a &eth1_mdio_sleep_pins_a>;
	pinctrl-names = "default", "sleep";
	phy-mode = "rgmii-id";
	max-speed = <1000>;
	phy-handle = <&phy1_eth1>;
	st,eth-clk-sel;
	snps,ext-systime;

	mdio1 {
		#address-cells = <1>;
		#size-cells = <0>;
		compatible = "snps,dwmac-mdio";
		phy1_eth1: ethernet-phy@4 {
			compatible = "ethernet-phy-id001c.c916";
			reset-gpios = <&gpioj 9 GPIO_ACTIVE_LOW>;
			reset-assert-us = <10000>;
			reset-deassert-us = <80000>;
			realtek,eee-disable;
			reg = <4>;
		};
	};
};

FYI, im working on a custom board with stm32mp257fai3 chip with custom ethernet 

1 reply

Olivier GALLIEN
ST Technical Moderator
Dec 11, 2025 10:23 AM UTC

Hi @sanjaysb 

 

Did you check wiki documentation starting from Ethernet overview - stm32mpu 

 

It might gives you useful information. 

 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.