Skip to main content
Associate III
Sep 29, 2025 7:28 PM UTC
Solved

DP83867 bring up issues - STM32MP131

Hi everyone,

 

I am trying to bring up the DP83867 with RGMII on the STM32MP131DAG7. However I am getting the following error:

[ 18.253959] stm32-dwmac 5800a000.ethernet end0: renamed from eth0
[ 23.695184] stm32-dwmac 5800a000.ethernet end0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 23.756147] stm32-dwmac 5800a000.ethernet end0: PHY [stmmac-0:00] driver [TI DP83867] (irq=POLL)
[ 24.764629] stm32-dwmac 5800a000.ethernet: Failed to reset the dma
[ 24.769435] stm32-dwmac 5800a000.ethernet end0: stmmac_hw_setup: DMA engine initialization failed
[ 24.808705] stm32-dwmac 5800a000.ethernet end0: __stmmac_open: Hw setup failed

 

I saw this is typically due to the 125MHz clock not being generated. In our schematic, we have the CLK_OUT from phy going to ETH_RGMII_CLK125. I noticed the phy was not generating a clock so using the "mii" tool in U-Boot, I tried to generate the clock by updating the 0x0170 register: Link I was unable to get any clock to generate even though the 25MHz clock was generated by crystal, all power rails were up, MDIO was communicating correctly, GTX_CLK was at 125MHz, and reset pin was not active (it seems driver never even tries to reset it). I gave up on this method and moved on to generating internally with RCC.

 

I updated the TF-A and OPTEE dts to generate the 125MHz clock as seen here:

root@stm32mp131-sga:~# cat /sys/kernel/debug/clk/clk_summary
pll3_q 1 1 0 125000000 0 0 50000 Y deviceless no_connection_id
 ck_ker_eth1 1 1 0 125000000 0 0 50000 Y deviceless no_connection_id
 eth1ptp_k 0 0 0 125000000 0 0 50000 Y deviceless no_connection_id
 eth1ck_k 1 1 0 125000000 0 0 50000 Y 5800a000.ethernet eth-ck

Updated the u-boot and kernel dts: (adding st, ext-phyclk)

eth1_rgmii_pins_mx: eth1-rgmii-mx-0 {
 pins1 {
 pinmux = <STM32_PINMUX('G', 13, AF11)>, /* ETH_RGMII_TXD0 */
 <STM32_PINMUX('G', 14, AF11)>, /* ETH_RGMII_TXD1 */
 <STM32_PINMUX('C', 2, AF11)>, /* ETH_RGMII_TXD2 */
 <STM32_PINMUX('E', 5, AF10)>, /* ETH_RGMII_TXD3 */
 <STM32_PINMUX('B', 11, AF11)>, /* ETH_RGMII_TX_EN */
 <STM32_PINMUX('C', 1, AF11)>, /* ETH_RGMII_GTX_CLK */
 //<STM32_PINMUX('F', 12, AF11)>, /* ETH_RGMII_CLK125 */
 <STM32_PINMUX('G', 12, AF11)>, /* ETH_PHY_INTN */
 <STM32_PINMUX('G', 2, AF11)>; /* ETH_MDC */
 bias-disable;
 drive-push-pull;
 slew-rate = <2>;
 };

 pins2 {
 pinmux = <STM32_PINMUX('G', 3, AF11)>; /* ETH_MDIO */
 bias-disable;
 drive-push-pull;
 slew-rate = <0>;
 };

 pins3 {
 pinmux = <STM32_PINMUX('C', 4, AF11)>, /* ETH_RGMII_RXD0 */
 <STM32_PINMUX('C', 5, AF11)>, /* ETH_RGMII_RXD1 */
 <STM32_PINMUX('B', 0, AF11)>, /* ETH1_RXD2 */
 <STM32_PINMUX('B', 1, AF11)>, /* ETH1_RXD3 */
 <STM32_PINMUX('A', 7, AF11)>; /* ETH_RGMII_RX_CTL */
 bias-disable;
 };
 };

 eth1_sleep_pins_mx: eth1_sleep_mx-0 {
 pins {
 pinmux = <STM32_PINMUX('G', 13, ANALOG)>, /* ETH1_TXD0 */
 <STM32_PINMUX('G', 14, ANALOG)>, /* ETH1_TXD1 */
 <STM32_PINMUX('C', 2, ANALOG)>, /* ETH_RGMII_TXD2 */
 <STM32_PINMUX('E', 5, ANALOG)>, /* ETH_RGMII_TXD3 */
 <STM32_PINMUX('G', 2, ANALOG)>, /* ETH1_MDC */
 <STM32_PINMUX('G', 3, ANALOG)>, /* ETH1_MDIO */
 <STM32_PINMUX('G', 12, ANALOG)>, /* ETH_PHY_INTN */
 <STM32_PINMUX('A', 7, ANALOG)>, /* ETH1_RGMII_RX_CTL */
 <STM32_PINMUX('B', 11, ANALOG)>, /* ETH1_TX_EN */
 <STM32_PINMUX('C', 4, ANALOG)>, /* ETH1_RXD0 */
 <STM32_PINMUX('C', 5, ANALOG)>, /* ETH1_RXD1 */
 <STM32_PINMUX('B', 0, ANALOG)>, /* ETH1_RXD2 */
 <STM32_PINMUX('B', 1, ANALOG)>, /* ETH1_RXD3 */
 <STM32_PINMUX('A', 11, ANALOG)>; /* ETH_RGMII_CLK */
 };
 };

 

&ethernet1 {
 status = "okay";
 pinctrl-0 = <&eth1_rgmii_pins_mx>;
 pinctrl-1 = <&eth1_sleep_pins_mx>;
 pinctrl-names = "default", "sleep";
 phy-mode = "rgmii-id";
 max-speed = <1000>;
 phy-handle = <&phy0_eth1>;
 phy-supply = <&scmi_vdd_system>;
 nvmem-cells = <&ethernet_mac1_address>;
 nvmem-cell-names = "mac-address";
 st,ext-phyclk;

 mdio {
 #address-cells = <1>;
 #size-cells = <0>;
 compatible = "snps,dwmac-mdio";
 phy0_eth1: ethernet-phy@0 {
 compatible = "ethernet-phy-id2000.a231";
 reg = <0>;
 reset-gpios = <&gpiod 5 GPIO_ACTIVE_LOW >;
 interrupt-parent = <&gpiog>;
 interrupts = <11 IRQ_TYPE_EDGE_FALLING>;
 ti,clk-output-sel = <DP83867_CLK_O_SEL_CHN_A_TCLK>;
 };
 };
};

 Using both methods I still get the same error message as above. I also tried different options for ti,clk-output-sel and the ti,tx/rx-internal-delay and commenting out reset gpios, but no difference.

 

In summary:

1. Tried to generate clock from phy, unable to do so

2. Generated 125MHz clock internally, same error message as before

 

Any guidance would be greatly appreciated as I feel I have tried every configuration.

devinschubert14Best answer
Associate III
Feb 4, 2026 6:50 PM UTC

Hi everyone,

 

After further debugging I noticed the phy was stuck in low power mode. As you can see in the schematic above, the INT/PWDN pin is only being pulled up to 1.8V and not 3.3V (datasheet says must be pulled to VDDIO) causing the phy to be stuck in this mode. After a rework, we now have full gigabit!

 

Thanks for the dts catch as well @Erwan SZYMANSKI , I am sure that would have been an issue later.

8 replies

Erwan SZYMANSKI
ST Technical Moderator
Oct 6, 2025 7:24 AM UTC

Hello @devinschubert14 ,
Do you have some schematics you are able to share ? At least the part between the SoC connections and the PHY ?
I see you tried a lot of different method and properties, but I think the best way is to focus on one goal you want to reach and investigate in this sense.

If you tried to generate the 125MHz from the outside (the PHY), I guess you have a 25MHz crystal in your design. You should so at probe time, see at one moment that this 125MHz clock comes in input of the SoC (ETHX_CLK125 pin).

Then you should check that ETH1_CLK_SEL value is well at 0 (Gates are manipulated by properties in device tree). The clock tree is documented in the RM (see below an extract):

 

ErwanSZYMANSKI_0-1759735297495.png

Do not hesitate to check too at this wiki article that can help: https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate III
Oct 6, 2025 6:33 PM UTC

Hi Erwan,

 

We originally tried to have the phy generate the 125MHz clock for the ETH1_RGMII_CLK125 pin, so let's keep trying in this direction.

 

I have followed the wiki article very closely. I do not have 125MHz clock coming from the PHY. I have looked with an oscope and there is no activity, however the 25MHz crystal is working. It seems the dp83867 driver never configures the 0x0170 register so it will never get the clock.

This setting is configured with:

ti,clk-output-sel = <DP83867_CLK_O_SEL_CHN_A_TCLK>;

I tried to use MDIO in u-boot to tell the phy to generate the clock by updating the 0x0170 register: Link I can see the register value is being updated, but the clock is still not generated.

I am aware of the ETH1_CLK_SEL which is set by the: st, ext-phyclk. If we are discussing having the phy generate the clock, this parameter should be removed from ethernet1 node in .dts.

 

I have done a ton of debugging so I am trying not to give too many details but I have tried many things.

 

Here is schematic:
SoC:

devinschubert14_1-1759774600289.png

 

Phy:

devinschubert14_2-1759774648284.png

 

Erwan SZYMANSKI
ST Technical Moderator
Oct 7, 2025 9:04 AM UTC

Hello @devinschubert14 ,
I begin to review the information you gave above. I just begin but I already see that the interruption described in the DTS under mdio node looks wrong isn't it ? 

According to your schematics, it seems that the interrupt is coming on PG12 but the device tree mentions PG11. PG11 looks like an unconnected pin.

[Edit: I see you declared it in pinctrl directly, but I do not understand so what is this interrupt declared in mdio node]

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate III
Feb 3, 2026 11:24 PM UTC

Hi @Erwan SZYMANSKI ,

 

I am still trying to fix this issue. I have given up on trying to get the phy clk from dp83867 and I have moved to:

RGMII with Crystal on PHY, no CLK125 from PHY (Reference clock (standard RGMII clock name) CLK125 is provided by a RCC SoC internal clock)

 

Current DTS:

	eth1_rgmii_pins_mx: eth1-rgmii-mx-0 {
		pins1 {
			pinmux = <STM32_PINMUX('G', 13, AF11)>, /* ETH_RGMII_TXD0 */
				 <STM32_PINMUX('G', 14, AF11)>, /* ETH_RGMII_TXD1 */
 <STM32_PINMUX('C', 2, AF11)>, /* ETH_RGMII_TXD2 */
				 <STM32_PINMUX('E', 5, AF10)>, /* ETH_RGMII_TXD3 */
				 <STM32_PINMUX('B', 11, AF11)>, /* ETH_RGMII_TX_EN */
				 <STM32_PINMUX('C', 1, AF11)>, /* ETH_RGMII_GTX_CLK */
				 //<STM32_PINMUX('F', 12, AF11)>, /* ETH_RGMII_CLK125 */
				 <STM32_PINMUX('G', 12, AF11)>, /* ETH_PHY_INTN */
				 <STM32_PINMUX('G', 2, AF11)>; /* ETH_MDC */
			bias-disable;
			drive-push-pull;
			slew-rate = <2>;
		};
		
		pins2 {
			pinmux = <STM32_PINMUX('G', 3, AF11)>; /* ETH_MDIO */
			bias-disable;
			drive-push-pull;
			slew-rate = <0>;
		};

		pins3 {
			pinmux = <STM32_PINMUX('C', 4, AF11)>, /* ETH_RGMII_RXD0 */
 <STM32_PINMUX('C', 5, AF11)>, /* ETH_RGMII_RXD1 */
 <STM32_PINMUX('B', 0, AF11)>, /* ETH1_RXD2 */
 <STM32_PINMUX('B', 1, AF11)>, /* ETH1_RXD3 */
 <STM32_PINMUX('A', 1, AF11)>, /* ETH1_RGMII_RX_CLK */
 <STM32_PINMUX('A', 7, AF11)>; /* ETH_RGMII_RX_CTL */
			bias-disable;
		};
	};

 

&ethernet1 {
	status = "okay";
	pinctrl-0 = <&eth1_rgmii_pins_mx>;
	pinctrl-1 = <&eth1_sleep_pins_mx>;
	pinctrl-names = "default", "sleep";
	phy-mode = "rgmii-id";
	max-speed = <1000>;
	phy-handle = <&phy0_eth1>;
	phy-supply = <&scmi_vdd_system>;
	nvmem-cells = <&ethernet_mac1_address>;
	nvmem-cell-names = "mac-address";
	st,ext-phyclk;	

	mdio {
		#address-cells = <1>;
		#size-cells = <0>;
		compatible = "snps,dwmac-mdio";
		phy0_eth1: ethernet-phy@0 {
 compatible = "ethernet-phy-id2000.a231";
			reg = <0>;
 reset-gpios = <&gpiod 5 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
 ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
 ti,tx-internal-delay = <DP83867_RGMIIDCTL_2_75_NS>;
		};
	};
};

 

I have noticed when I get to kernel, the GPIO is set to low and then remains there after DMA reset fails. In U-Boot, the reset pin is deasserted and I am able to use mii tool, but DMA reset fails. I get the same error in U-Boot and Kernel where the DMA fails to reset. 

 

I also used devmem2 to check the syscfg parameters and confirmed that eth_clk_sel = 1 and eth_ref_clk_sel = 0. I also followed this link and added the include to my dts but did not fix: https://community.st.com/t5/stm32-mpus-products-and-hardware/dp83867-phy-clock-problem-don-t-bring-up/td-p/208675

 Is there any way to get more debug details from the stmmac or dp83867 driver? 

devinschubert14AuthorBest answer
Associate III
Feb 4, 2026 6:50 PM UTC

Hi everyone,

 

After further debugging I noticed the phy was stuck in low power mode. As you can see in the schematic above, the INT/PWDN pin is only being pulled up to 1.8V and not 3.3V (datasheet says must be pulled to VDDIO) causing the phy to be stuck in this mode. After a rework, we now have full gigabit!

 

Thanks for the dts catch as well @Erwan SZYMANSKI , I am sure that would have been an issue later.