Skip to main content
Lead
Apr 21, 2026 12:49 PM UTC
Question

Does Linux block USART6 early debug output when starting?

I have an issue were the Linux kernel is booting, then it just stops printing out messages from USART6.

Meanwhile, optee, u-boot and TF-a is printing out messages from USART6. But not Linux after a while.

What can have caused this?

My processor is: STM32MP257F.

6 replies

Erwan SZYMANSKI
ST Technical Moderator
Apr 22, 2026 12:52 PM UTC

Hello @DMårt ,
Are you sure you don't have a firmware running on M33 that uses or just reconfigure the USART6 instance ? The fact that you have the logs at the beginning but disappear after some time let me think about a such possibility.

[Edit: if not, the USART6 is certainly well configured in earliest boot stages, and Linux does not keep a good configuration on it, but maybe more logs could help to understand exactly where does it disappear]

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
DMårtAuthor
Lead
Apr 22, 2026 9:11 PM UTC

Hi @Erwan SZYMANSKI 

Here is the log.

As you can see

vddio2: disabling
vddio3: disabling
vddio4: disabling
vddcore: disabling
v1v8: disabling
v3v3: disabling

I don't know why this is happening inside Linux. 

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
Erwan SZYMANSKI
ST Technical Moderator
Apr 27, 2026 12:36 PM UTC

Hello @DMårt ,
I think you have a misalignment between your kernel version and your other OpenSTLinux BSP components.

I just felt on this issue by pure chance when working on another topic. It was due to my BSP on OpenSTLinux v6.2 (OP-TEE, TF-A, U-Boot), while my kernel was in OSTL 6.1.

Please double check this.

The blocking point is not the USART at all, but in your complete log, you see the RCC probe is broken:

[ 6.578092] stm32mp25_rcc 44200000.clock-controller: Can't register clk 2: -17
[ 6.583185] stm32 clock failed to initialize
[ 6.587482] stm32mp25_rcc: probe of 44200000.clock-controller failed with error -17

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.