Skip to main content
KChoj.2312
Associate II
Dec 9, 2019 11:29 PM UTC
Question

Device Tree configuration form GPIO

Hi,

Is there any example showing how to configure a simple GPIO line using DeviceTree? I would like to set the pullup/pulldown or open drain and then use the /sys/class/gpio to read or write the value. The only example I can find is the GPIO setting for particular peripheral and not for standalone input/output pin.

I have added the following section to the &pinctrl in my device tree but I think it has no effect on the pins configuration.

	gpio_pins_mx: gpio_pins_mx-0 {
		u-boot,dm-pre-reloc;
		pins {
			u-boot,dm-pre-reloc;
			pinmux = <STM32_PINMUX('D', 11, GPIO)>,
				<STM32_PINMUX('C', 0, GPIO)>,
				<STM32_PINMUX('B', 7, GPIO)>;
			bias-pull-down;
		};
	};

Thank you,

Chris

This topic has been closed for replies.

5 replies

Olivier GALLIEN
ST Technical Moderator
Dec 12, 2019 10:16 AM UTC

Hi @Community member​ 

Did you refer to https://wiki.st.com/stm32mpu/wiki/GPIO_device_tree_configuration ?

Did you check same pin are not used / configured for another peripheral ?

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
KChoj.2312
Associate II
Dec 12, 2019 10:44 AM UTC

Yes, I know this document, but is it not clear to me how i should configure the standalone GPIO. The article specifies the foo-device that controls the GPIO, however I need to configure a GPIO for the independent control with the /sys/class/gpio subsystem. The pins I listed are not used by any other device, but I suspect that I need to refer to them in the root node somehow.

I am able to control the GPIO by exporting them and using the direction and value files, however i still don't know hot to set the pull-ups etc.

Chris

rhaberkorn
Associate II
Oct 10, 2022 1:34 AM UTC

I would also be interested in this. The only answer I found so far is writing a dummy driver existing solely, so we can declare something in the device tree and reference the pinctrl node for our GPIO. There has got to be a simpler solution.

Associate III
Jan 20, 2025 12:36 PM UTC

@KChoj.2312 

@rhaberkorn 

Are you solved yours problem ?

I would like to configure a GPIO for the independent control with the /sys/class/gpio subsystem, example pin PH11 ?

How should  looks *.dts file ?

rhaberkorn
Associate II
Jan 20, 2025 8:31 PM UTC

@ienecodeNo. I worked around it by writing a systemd service that uses gpioset on startup.