Skip to main content
asadullah4571
Associate III
Oct 8, 2024 8:48 AM UTC
Question

Custom board (stm32mp1) JTAG connecting issue

Hi
In my custom board (stm32mp157F) i added the JTAG , i try to connect JTAG for flashing the firmware into the M4 processor, i change the boot pins as Engineering mode, but not connected to cub programmer as well as cube IDE.

i attached the screenshot of the Schematic diagram of JTAG. 
please let me know where i am missing.

asadullah4571_0-1728377155069.pngasadullah4571_1-1728377186695.png

 


 

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
Oct 8, 2024 8:58 AM UTC

Hi @asadullah4571 ,

On STM32MPx MPUs products, unlike STM32 MCUs, the JTAG/SWD cannot be used for flashing.

Only USB or UART could be used with CubeProgrammer.

Furthermore, note that there is no embedded Flash and Cortex-M4 only run from internal SRAMs loaded by Cortex-A7 (uBoot or Linux) during runtime.

JTAG/SWD is only used for debug purpose. CubeIDE could be used to debug Cortex-M4 FW in either production mode (i.e. Linux up and running) or development boot (aka Engineering boot).
https://wiki.st.com/stm32mpu/wiki/STM32CubeIDE#Arm-C2-AE_Cortex-C2-AE-M_debug_on_STM32_MPU_device

 

Regards.

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent