Skip to main content
Mark81
Associate III
Apr 15, 2020 8:21 AM UTC
Question

create_emmc_from_flashlayout.sh

With the Distribution Package for STM32MP1 I created my own machine (STM32MP151A) and I was able to generate a the flashlayout for both sdcard and emmc.

I don't see any script to create the image for emmc, like `create_sdcard_from_flashlayout.sh`.

Is there such a template or I am on my own?

This topic has been closed for replies.

2 replies

PatrickF
ST Employee
Apr 15, 2020 8:33 AM UTC

Hi,

The SD-Card image is only required when you program SD-Card out of the target, e,g, on a Linux PC using dd command.

https://wiki.st.com/stm32mpu/wiki/How_to_populate_the_SD_card_with_dd_command

As the eMMC is soldered, it is intended to be programmed on-board using CubeProgrammer (via USB), so only a flashlayout (.tsv) is needed.

If you wish to program eMMC before soldering it (usually only for large production scale), it is up to you to create the image suited for your programming system.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Mark81
Mark81Author
Associate III
Apr 15, 2020 9:29 AM UTC

Hi! Both solutions are not applicable here. We want to do the following:

  1. boot the target with the sd-card
  2. copy (aka dd) the emmc image into the device (I see it as /dev/mmcblk2)
  3. reboot from the emmc removing the sd-card

This will allow also an easy way to update the software if needed.

For this reason I want to create the raw image. I saw that changing the script setting mmc1 as device will produce an "emmc" image.

Do you think it's ok my idea?