Skip to main content
jgauthier
Senior
Nov 3, 2021 3:27 PM UTC
Question

Compiler Bug?

I ran into a warning for one section of code that I did not for a different section of code. So I simplified it into two function. I don't see why I get a warning for one and not the other.

void test32(uint32_t *data) {
	uint32_t src_addr = (uint32_t) data;
}
 
void test16(uint16_t *data) {
	uint16_t src_addr = (uint16_t) data;
}

The compiler complains (also about unused variables, but I removed those)

../Core/Src/main.c: In function 'test16':
../Core/Src/main.c:161:22: warning: cast from pointer to integer of different size [-Wpointer-to-int-cast]
 161 | uint16_t src_addr = (uint16_t) data;
 | ^
 

The compiler appears to be based on gcc 9.3.1.

If I put these two functions in a simple C file and build it on straight Linux (gcc 9.3.0) the warning exists for both instances.

main.c: In function ‘test16’:
main.c:15:23: warning: cast from pointer to integer of different size [-Wpointer-to-int-cast]
 15 | uint16_t src_addr = (uint16_t) data;
 | ^
main.c: In function ‘test32’:
main.c:20:23: warning: cast from pointer to integer of different size [-Wpointer-to-int-cast]
 20 | uint32_t src_addr = (uint32_t) data;
 | ^
 

This topic has been closed for replies.

5 replies

KnarfB
Super User
Nov 3, 2021 3:29 PM UTC

64-bit Linux? This would explain the difference.

hth

KnarfB

jgauthier
jgauthierAuthor
Senior
Nov 3, 2021 3:31 PM UTC

Yes, x64 linux. I don't understand the difference between the two variables types on stm32, and why that warning comes up.

KnarfB
Super User
Nov 3, 2021 3:39 PM UTC

sizeof a pointer is 8 bytes on a 64-bit Linux but 4 bytes on a 32-bit STM. Therefore test32 yields a the warning under Linux but not on STM (same size like uint32_t).

jgauthier
jgauthierAuthor
Senior
Nov 3, 2021 3:41 PM UTC

I see. It's the pointer size. Okay, thanks!

MM..1
Super User
Nov 3, 2021 5:08 PM UTC

And for detail test16 is failure ... truncate part from pointer.