Skip to main content
PVaaz.1
Associate III
Aug 19, 2022 6:25 PM UTC
Question

Communication between STM32MP1 A7 and STM32 over SPI

Hello ,

Can anyone please point me to the example of SPI communication between stm32(F4/L0/L4) with A7 of STM32MP1?

A7 could be a driver or any user application but both should be able to send and receive the data over spi.

on A7 I suppose it will be SPI5.

please assist.

Thanks in advance!

Br,,

P

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
Sep 1, 2022 1:02 PM UTC

Hi @PVaaz.1​ 

is those pages help you for a start point ?

https://wiki.st.com/stm32mpu/wiki/SPI_overview#API_description

https://wiki.st.com/stm32mpu/wiki/How_to_use_SPI_from_Linux_userland_with_spidev

Regards

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent