Skip to main content
Associate II
Mar 25, 2026 5:42 PM UTC
Solved

cant put PZ3 into interrupt mode

gpioinfo output

gpiochip9 - 10 lines:
line 0: "PZ0" input
line 1: "PZ1" input
line 2: "PZ2" input
line 3: "PZ3" input

gpiomon output

# gpiomon --num-events 1 --edges falling PZ0
^C
# gpiomon --num-events 1 --edges falling PZ1
^C
# gpiomon --num-events 1 --edges falling PZ2
^C
# gpiomon --num-events 1 --edges falling PZ3
gpiomon: unable to request lines on chip /dev/gpiochip9: No such device or address

why is there a problem with PZ3 pin specifically? noone is using it

should i add something in dts?

PatrickF
PatrickFBest answer
ST Employee
Mar 26, 2026 7:29 AM UTC

Hi @vdl 

Most probable cause if because you already have another GPIO Px[3] defined as interrupt elsewhere.

This is a general constrains on most STM32 products due to the way the interrupt mux is done wrt GPIOs pins. Please refer to Reference Manual for details.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

2 replies

PatrickF
PatrickFBest answer
ST Employee
Mar 26, 2026 7:29 AM UTC

Hi @vdl 

Most probable cause if because you already have another GPIO Px[3] defined as interrupt elsewhere.

This is a general constrains on most STM32 products due to the way the interrupt mux is done wrt GPIOs pins. Please refer to Reference Manual for details.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
vdlAuthor
Associate II
Mar 26, 2026 7:57 AM UTC

disabled emmc1 ( sd card interface ) which was using PD3 as interrupt - now PZ3 works

weirdly i still can gpiomon PD3 and other Px3 pins ( unused ones )

also i could gpiomon other Px3 before