Skip to main content
KMark.1
Associate
May 7, 2025 11:44 AM UTC
Solved

Can't boot a trusted image for stm32mp157f-dk2 board

Moved from MCUs form - STM32MP are MPUs, not MCUs.


NOTICE: CPU: STM32MP157FAC Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157F-DK2 Discovery Board
NOTICE: Board: MB1272 Var4.0 Rev.C-02
NOTICE: Bootrom authentication failed
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffdd000
INFO: FCONF: Reading firmware configuration information for: cot_desc
INFO: FCONF: Reading firmware configuration information for: tbbr
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.6-stm32mp1-r2.1(release):v2.6-dirty(a1f02f4f)
NOTICE: BL2: Built : 13:14:26, Nov 23 2021
NOTICE: TRUSTED_BOARD_BOOT support enabled
INFO: Using crypto library 'stm32_crypto_lib'
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2: Loading image id 1
INFO: Loading image id=17 at address 0x2ffff000
INFO: Image id=17 loaded: 0x2ffff000 - 0x2ffff369
NOTICE: ROTPK is not deployed on platform. Skipping ROTPK verification.
INFO: Loading image id=1 at address 0x2ffff000
INFO: Image id=1 loaded: 0x2ffff000 - 0x2ffff226
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=14 at address 0x2ffc5000
INFO: Image id=14 loaded: 0x2ffc5000 - 0x2ffc536c
NOTICE: ROTPK is not deployed on platform. Skipping ROTPK verification.
INFO: Loading image id=4 at address 0x2ffc5000
INFO: Image id=4 loaded: 0x2ffc5000 - 0x2ffd75d8
INFO: BL2: Skip loading image id 8
INFO: BL2: Skip loading image id 9
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0xc0500000
INFO: Image id=2 loaded: 0xc0500000 - 0xc051dcc8
INFO: BL2: Loading image id 16

Data Abort at: 0x2ffe50c4 DFSR = 0x00000206 DFAR = 0x00000008

Abort at: 0x2ffe439c

The above is the boot log for trusted image for stm32mp157f. I am able to boot Optee image for the same. I am using yocto(kirkstone) to build image. The image is secure boot enable. I am not sure why data abort is happening.

This topic has been closed for replies.
Roger SHIVELY
Roger SHIVELYBest answer
ST Employee
May 7, 2025 8:30 PM UTC

Hello @KMark.1 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

Regards,

Roger

3 replies

Roger SHIVELY
Roger SHIVELYBest answer
ST Employee
May 7, 2025 8:30 PM UTC

Hello @KMark.1 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

Regards,

Roger

KMark.1
KMark.1Author
Associate
May 13, 2025 5:08 AM UTC

@Roger SHIVELY  Any update on this post

Olivier GALLIEN
ST Technical Moderator
Jun 16, 2025 7:55 AM UTC

Issue closed in OLS. 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.