Skip to main content
nataut
Associate III
May 12, 2023 8:53 AM UTC
Solved

bitbake build errors

Hi All.

I'm attempting to build an OpenSTLinux based software using a virtual machine VMWARE UBUNTU 16.2.5 build-20904516

Using the command "bitbake -v -k <my_recipe_bb_name_file>" i have the error message: " ERROR: Nothing PROVIDES '–v' "

Using the command "bitbake -k <my_recipe_bb_name_file>" i have the error message: " ERROR: Nothing PROVIDES '–k' "

Using the command "bitbake <my_recipe_bb_name_file>" i have not errors but the compilation after many houres fails 

Using the command "bitbake -c cleanall <my_recipe_bb_name_file>" i have the error message: " ERROR: Nothing PROVIDES '–c' "

If I use another PC with the same virtual machine and the same "layers" folder, I have no errors

Why? 

Thanks

This topic has been closed for replies.
nataut
natautBest answer
Associate III
May 12, 2023 9:21 AM UTC

I found the problem.

The symbol in “–v�? and "–k", before "v" and "k" has to be “-“ and not �?–“.

Thanks

4 replies

nataut
natautAuthorBest answer
Associate III
May 12, 2023 9:21 AM UTC

I found the problem.

The symbol in “–v�? and "–k", before "v" and "k" has to be “-“ and not �?–“.

Thanks

Olivier GALLIEN
ST Technical Moderator
May 12, 2023 9:40 AM UTC

Hi @nataut​ 

VMWARE 16.2.5 build-20904516 -> is the version of your VMware Workstation.

Which Ubuntu LTS you run ?

With OpenSTLinux release ?

Thanks,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
nataut
natautAuthor
Associate III
May 12, 2023 9:54 AM UTC

Hi ​@Community member​  

Ubuntu 16.04 LTS

OpenSTLinux 4.19-thud-mp1-19-02-20

Thanks

Olivier GALLIEN
ST Technical Moderator
May 12, 2023 9:56 AM UTC

I missed your previous comment. Good you find the issue.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.