Skip to main content
Niklas Voi
Associate II
May 5, 2020 2:19 PM UTC
Question

Added Custom Board from CubeMx, but an error occour

Hi St-Community,

im hanging around with the following Problem:

I build up a yocto environment and build sucessfully images. No its time to add a custom devicetree to the linux.

So i followed the instructions on:

https://wiki.st.com/stm32mpu/wiki/How_to_create_your_own_machine

But i get the following error when i start to build a image with bitbake image-base-minimal.

ERROR: u-boot-stm32mp-extlinux-2.0-r0 do_create_multiextlinux_config: No UBOOT_EXTLINUX_CONFIG_FLAGS list defined, nothing to do
ERROR: u-boot-stm32mp-extlinux-2.0-r0 do_create_multiextlinux_config: Function failed: update_extlinuxconf_targets
ERROR: Logfile of failure stored in: /opt/build/tmp/work/stm32mp1_mustera-poky-linux-gnueabi/u-boot-stm32mp-extlinux/2.0-r0/temp/log.do_create_multiextlinux_config.5058
ERROR: Task (/opt/yocto/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp-extlinux.bb:do_create_multiextlinux_config) failed with exit code '1'

Have you any hints to me where i can debug. I dont know wehere these variables are defined.

Best regards and many thanks

Niklas

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
May 6, 2020 7:33 AM UTC

Hi @Niklas Voi​ 

There is no recipe image-base-minimal, do you mean st-image-core or core-image-minimal ?

May you share your stm32mp1-<ProjectName>.conf for further help ?

Thanks

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Niklas Voi
Associate II
May 6, 2020 8:13 AM UTC

Hi Oliver,

here is my machine:

#@TYPE: Machine
#@NAME: stm32mp1-mustera
#@DESCRIPTION: Configuration for STM32CubeMX generated project
#@NEEDED_BSPLAYERS: layers/meta-openembedded/meta-oe layers/meta-openembedded/meta-python
 
include conf/machine/include/st-machine-common-stm32mp.inc
include conf/machine/include/stm32mp1-mx-config.inc
include conf/machine/include/stm32mp1-mx-extlinux-config.inc
include conf/machine/include/stm32mp1-mx-common.inc
 
# =========================================================================
# CubeMX extra config
# =========================================================================
# Set specific path by components for DT file location
CUBEMX_DTB_PATH_TFA = "${STM32MP_MX_BASE}/mx/${CUBEMX_PROJECT}/tf-a"
CUBEMX_DTB_PATH_UBOOT = "${STM32MP_MX_BASE}/mx/${CUBEMX_PROJECT}/u-boot"
CUBEMX_DTB_PATH_LINUX = "${STM32MP_MX_BASE}/mx/${CUBEMX_PROJECT}/kernel"
CUBEMX_DTB_PATH_OPTEEOS = "${STM32MP_MX_BASE}/mx/${CUBEMX_PROJECT}/optee-os"
 
# =========================================================================
# User customizing sections
# =========================================================================
 
# Boot Scheme
# =========================================================================
# DISCO / EVAL : basic, trusted or optee
# =========================================================================
#BOOTSCHEME_LABELS += "basic"
BOOTSCHEME_LABELS += "trusted"
#BOOTSCHEME_LABELS += "optee"
 
# Boot Device Choice
# =========================================================================
# DISCO : sdcard
# EVAL : sdcard, emmc, nand-4-256, nor-sdcard, nor-emmc or nor-nand-4-256
# =========================================================================
# Define the boot device supported
BOOTDEVICE_LABELS += "sdcard"
 
# WARNING: configs below are only available with EVAL board
#BOOTDEVICE_LABELS += "emmc"
#BOOTDEVICE_LABELS += "nand-4-256"
#BOOTDEVICE_LABELS += "nor-emmc"
#BOOTDEVICE_LABELS += "nor-nand-4-256"
#BOOTDEVICE_LABELS += "nor-sdcard"
 
# Board Type Choice
# =========================================================================
# DISCO : stm32mp157a-dk1 or stm32mp157c-dk2
# EVAL : stm32mp157c-ev1
# =========================================================================
# Define the board reference devicetree name
# WARNING: only one setting allowed
#CUBEMX_BOARD_REFERENCE = "stm32mp157a-dk1"
CUBEMX_BOARD_REFERENCE = "stm32mp157c-dk2"
#CUBEMX_BOARD_REFERENCE = "stm32mp157c-ev1"
 
# CubeMX Project Config
# =========================================================================
# Assign CubeMX Board devicetree and project path name
CUBEMX_DTB = "stm32mp157c-cube-project-for-muster-a-mx"
CUBEMX_PROJECT = "MusterA"

I mean core-image-minimal to build. I have started with a blank yocto and than added the layers:

/opt/yocto/
├── clean_repos.sh
├── meta-openembedded
├── meta-squirrel # Here is our company stuff, so ignore this
├── meta-st-stm32mp
├── meta-st-stm32mp-addons
└── poky

Builduing for the DK2 works fine.

Thanks for your help :)

Niklas