Skip to main content
Niklas Voi
Associate II
May 19, 2020 2:14 PM UTC
Question

Activating UART3 for Linux not possible. Are there any hints for me, where to look?

Hi Folks,

i created a custom dts and build it via the mx-addons howto. My goal is to activate USART3 on DK2.

For USART3 is create the following source in the DT:

&usart3{
	pinctrl-names = "default", "sleep", "idle";
	pinctrl-0 = <&usart3_pins_a>;
	pinctrl-1 = <&usart3_sleep_pins_a>;
	pinctrl-2 = <&usart3_idle_pins_a>
	status = "okay";
 
	/* USER CODE BEGIN usart3 */
	/* USER CODE END usart3 */
};
 
	usart3_pins_mx: usart3_mx-0 {
		u-boot,dm-pre-reloc;
		pins1 {
			u-boot,dm-pre-reloc;
			pinmux = <STM32_PINMUX('B', 10, AF7)>, /* USART3_TX */
					 <STM32_PINMUX('G', 8, AF8)>; /* USART3_RTS */
			bias-disable;
			drive-push-pull;
			slew-rate = <0>;
		};
		pins2 {
			u-boot,dm-pre-reloc;
			pinmux = <STM32_PINMUX('B', 12, AF8)>, /* USART3_RX */
					 <STM32_PINMUX('B', 13, AF7)>; /* USART3_CTS */
			bias-disable;
		};
	};
 
	usart3_sleep_pins_mx: usart3_sleep_mx-0 {
		u-boot,dm-pre-reloc;
		pins {
			u-boot,dm-pre-reloc;
			pinmux = <STM32_PINMUX('B', 10, ANALOG)>, /* USART3_TX */
					 <STM32_PINMUX('B', 12, ANALOG)>, /* USART3_RX */
					 <STM32_PINMUX('B', 13, ANALOG)>, /* USART3_CTS */
					 <STM32_PINMUX('G', 8, ANALOG)>; /* USART3_RTS */
		};
	};
 
	/* USER CODE BEGIN pinctrl */
	/* USER CODE END pinctrl */
};

And i get in the bootmessage:

[ 0.430813] stm32-dma 48000000.dma: STM32 DMA driver registered
[ 0.432952] stm32-dma 48001000.dma: STM32 DMA driver registered
[ 0.514748] STM32 USART driver initialized
[ 0.516149] stm32-usart 4000e000.serial: Linked as a consumer to 48000000.dma
[ 0.516515] 4000e000.serial: ttySTM3 at MMIO 0x4000e000 (irq = 24, base_baud = 4000000) is a stm32-usart
[ 0.516810] serial serial0: tty port ttySTM3 registered
[ 0.516877] genirq: irq_chip stm32-exti-h did not update eff. affinity mask of irq 72
[ 0.517785] stm32-usart: probe of 4000f000.serial failed with error -22
[ 0.518837] stm32-usart 40010000.serial: interrupt mode used for rx (no dma)
[ 0.518863] stm32-usart 40010000.serial: interrupt mode used for tx (no dma)
[ 0.518892] 40010000.serial: ttySTM0 at MMIO 0x40010000 (irq = 26, base_baud = 4000000) is a stm32-usart
[ 1.463868] console [ttySTM0] enabled

The USART3 is at 400f000 so i get these error 22.

Does any one has any hints for me where to look?

Best regards and thanks,

Niklas

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
May 19, 2020 2:34 PM UTC

Hi @Niklas Voi​ 

Do you know those links :

https://wiki.st.com/stm32mpu/wiki/Serial_TTY_device_tree_configuration

https://wiki.st.com/stm32mpu/wiki/Trace_and_debug_scenario_-_UART_issue

Better to double check if dts generated by CubeMX does not need to be manually customized, and then use debug technics to try to understand what's going on.

Hope it help

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.