Skip to main content
MCho.1
Visitor II
Jun 12, 2020 12:07 AM UTC
Question

A project created by X-Cube-Ai 5.1.0 on STM32MP157-DK2 is stuck in an infinite loop.

0693W000001qYX7QAM.png

 

 

 

 

I just made a pure x-cube-ai project with no user code included, and it is stuck at creating network object... I couldn't analyze this problem because it seems to be related to the network library.(prefix .a). Willing to help me out?

This topic has been closed for replies.

1 reply

fauvarque.daniel
ST Employee
Jun 12, 2020 12:59 PM UTC

You need to enable CRC2 on the CortexM4 context of the MP1 to make it work

As of today systemperformance and validation on the target only works in engineering mode as they require a USART connection to the host via the stlink.

We are working on a more integrated solution.

Regards

Daniel

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.