Skip to main content
Emmanuel COMBETTE DE RYMON
ST Employee
May 28, 2020 8:59 AM UTC

FAQ: Application notes on STM32MPU power distribution

There are different power supply design solutions possible to supply the STM32MPx microprocessors.

For the supply of the microprocessor, ST recommends the dedicated power management IC, the STPMIC1 for the STM32MP1x family and STPMIC25 or STPMIC2L for the STM32MP2x family.

The STPMICx chip gathers all the required supplies of the STMP32MPx, with the expected power ON/OFF or low-power sequences. STPMICx chip offers a smaller footprint on the design compare to design with discrete power supplies.

With the STM32MP2 family, a discrete power supply solution is not recommended due to complexity. 

To see different design examples of platform power distributions, view the application note depending on the STM32MPx family:

AN5031: Getting started with STM32MP151, STM32MP153 and STM32MP157 line hardware development

  • STPMIC1A with STM32MP1 VDD IOs  = 3V3 with a DDR3L
  • STPMIC1B with STM32MP1 VDD IOs  = 1V8 with an LPDDR2
  • Power supply with discrete supplies STM32MP1 VDD IOs  =  3V3 or 1V8 with DDR3L

AN5489: Getting started with STM32MP25x MPUs hardware development

  • STPMIC25A with STM32MP25 VDD IOs  = 3V3 with a DDR4
  • STPMIC25B with STM32MP25 VDD IOs  = 1V8 with an LPDDR4

AN6055: Getting started with STM32MP21x lines hardware development

  • STPMIC2LA with STM32MP21 VDD IOs  = 3V3 with a DDR4
  • STPMIC2LB with STM32MP21 VDD IOs  = 1V8 with an LPDDR4


To get a system overview (with STM32MPu, STPMICx, DRAM, boot flash device) ST offers an illustration through a complete application example in below application note. These documents provide many system information about power up/down, low-power sequences, USB management.

We recommend the following application notes:

The application note below ensures the low-power use-cases and is battery-oriented, includes USB, battery charger, eMMC, SD card boot devices.

In these application notes below, the application is supplied by an external wall adapter supply.

The application notes below provide the same system level information for power distribution with discrete power supplies. This applies to applications that do not embed the STPMIC1x.

A complete overview of relevant application notes is available in the ST Wiki:

This topic has been closed for replies.