ZigBee Coordinator on STM32WB5MMG with Off-The-Shelf devices
Hi All,
I am quite a newby regarding ZigBee since I have been playing around with this since bare a month now. So please be patient if my question might sound stupid or my terminology is not quite "ZigBee-conform".
Short form of my question: Why do non of my off-the-shelf ZigBee devices report to my Coordininator? I guess there is additional code required, but which?
Long form and some background:
I try to associate a off-the-shelf device with a ZigBee-Coordinator. The Coordinator is created on a STM32WB55MMG module with STM32CubeMX. The coordinator starts up well and I get all the debug output I expected. But when I try to associate an off-the-shelf device, it seems to fail.
I implemented the following clusters on Endpoint 1 of my Coordinator device, by checking the appropriate boxes in the STM32CubeMX/Middleware/STM32_WPAN:
Basic (Server)
Identify (Server/Client)
Groups (Server)
On/Off /Server, all callbacks checked)
LevelControl (Server, all callbacks checked)
The reason why I did choose these clusters are the devices I want to connect.
It tested with different devices:
SonOff Wireless Switch SNZB-01
IKEA Tradfri Shortcut Button Typ E1812
All these devices work well with a ZigStar4 USB dongle and ZigBee2MQTT.
But when I start the network forming process with my STM32WB5MMG as coordinator all I get is this log output, an non of the cluster callback functions get called:
[M4 APPLICATION] APP_ZIGBEE_Init
[M4 APPLICATION] **********************************************************
[M4 APPLICATION] WIRELESS COPROCESSOR FW:
[M4 APPLICATION] VERSION ID = 1.13.2
[M4 APPLICATION] FW Type : FFD Zigbee stack
[M4 APPLICATION] Application flashed: ..
[M4 APPLICATION] Channel used: 11
[M4 APPLICATION] Link Key: ZigBeeAlliance09
[M4 APPLICATION] Link Key value: 5a 69 67 42 65 65 41 6c 6c 69 61 6e 63 65 30 39
[M4 APPLICATION] Clusters allocated are:
[M4 APPLICATION] OnOff Server on Endpoint 1
[M4 APPLICATION] **********************************************************
[M0] [00000000.000][API] Init_ZigbeeStack_Infrastructure
[M4 APPLICATION] APP_ZIGBEE_StackLayersInit
[M4 APPLICATION] Network config : APP_STARTUP_CENTRALIZED_COORDINATOR
[M0] [00000000.019][PLATFORM] ZbNlmeResetReq : NLME-RESET.request (warmStart = 0)
[M0] [00000000.014][PLATFORM] nwk_scan_req : MLME-SCAN.request (wpan0): type=1, page=0, mask=0x00000800, dur=4
[M0] [00000000.278][API] Scan Done - unscan channels 0x0
[M0] [00000000.279][PLATFORM] nwk_scan_req : MLME-SCAN.request (wpan0): type=0, page=0, mask=0x00000800, dur=4
[M0] [00000000.542][API] Scan Done - unscan channels 0x0
[M0] [00000000.543][PLATFORM] nwk_pick_quietest_channel : Found starting channel at 11 (num devices = 1, energy = 255)
[M0] [00000000.545][PLATFORM] MLME-START.confirm : ifc:wpan0, channel:11, page: 0, pan:0x6449, status:0x00
[M0] [00000000.546][PLATFORM] nwk_handle_scan_conf_form_energy : NLME-NETWORK-FORMATION.request successful (nwkPanId = 0x6449).
[M4 APPLICATION] ZbStartup Callback (status = 0x00)
[M0] [00000016.048][PLATFORM] nwk_handle_assoc : Association accepted, sending response (0xbcf9, 0x00124b0022658937)
[M0] [00000031.469][PLATFORM] nwk_leave_send_cmd : Sending leave command for 0x00124b0022658937.
[M0] [00000083.925][PLATFORM] nwk_handle_assoc : Association accepted, sending response (0x5db2, 0x540f57fffef592e8)
[M0] [00000086.036][PLATFORM] nwk_handle_assoc : Association accepted from previous child (0x5db2, 0x540f57fffef592e8)The 0x00124b0022658937 is the SonOff device and the 0x540f57fffef592e8 is the IKEA.
Any hints or ideas what I am missing to successfully integrate one of these devices into my ZigBee network? Thank you all for any help!
Best Regards
Thomas